IDT to Showcase Magnetic Induction- and Resonance-based Wireless Power Solutions at 2013 International Consumer Electronics Show in Las Vegas, January 8-11

January 3, 2013

SAN JOSE, Calif., January 3, 2013 – Integrated Device Technology, Inc. (IDT®; NASDAQ: IDTI), the Analog and Digital Company™ delivering essential mixed-signal semiconductor solutions, today announced that it will be exhibiting its industry-leading wireless power solutions at the 2013 International Consumer Electronics Show (CES) in Las Vegas, January 8-11. CES provides an ideal venue to showcase IDT’s solutions, which are suited for a myriad of mobile applications for convenient and effortless battery charging. 

          “We are excited to demonstrate our award-winning wireless power products and next-generation solutions at CES,” said Arman Naghavi, vice president and general manager at IDT. “Wireless power is an important element of IDT’s power management strategy. Recently announced partnerships and the development of magnetic induction and magnetic resonance solutions have quickly established IDT as a leader in this market. We are building upon our early successes with continued innovation that provides our customers with the solutions they need to develop the most advanced next-generation consumer electronics.”

          IDT will exhibit the world’s first true single-chip wireless power transmitter (IDTP9030) and highest-output-power single-chip receiver solution (IDTP9020). The high-level of integration enables system designers to significantly reduce component count, board area, and cost to deliver superior wireless charging products in convenient and attractive form factors. Both devices comply with the Wireless Power Consortium (WPC) Qi standard, which ensures interoperability with any other device meeting the WPC Qi standard. Both transmitter and receiver are capable of “multi-mode” operation, supporting both the Qi standard as well as proprietary formats for added features, increased power output capability, and improved safety.

          In addition, IDT will showcase the recently-announced IDTP9035 and IDTP9036 wireless power transmitter solutions, designed to meet the WPC Tx-A5, Tx-A6, and Tx-A11 configurations. The new products expand IDT’s portfolio of WPC Qi-compliant transmitters with solutions optimized for single-coil 5 V and three-coil 12 V applications.

          IDT has partnered with both Intel and Qualcomm to develop wireless charging solutions for magnetic resonance-based charging technology. IDT is also a member of the Alliance for Wireless Power (A4WP), an independently operated organization composed of global wireless power and technology industry leaders. Next-generation magnetic resonance-based solutions will be on display at the show. For more information about IDT’s wireless power solutions, visit www.wirelesspowerbyidt.com.

About IDT

          Integrated Device Technology, Inc., the Analog and Digital Company™, develops system-level solutions that optimize its customers’ applications. IDT uses its market leadership in timing, serial switching and interfaces, and adds analog and system expertise to provide complete application-optimized, mixed-signal solutions for the communications, computing and consumer segments. Headquartered in San Jose, Calif., IDT has design, manufacturing and sales facilities throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT is accessible at www.IDT.com. Follow IDT on FacebookLinkedInTwitter, and YouTube.

###

IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.