Patented 3-State Technique Improves Efficiency, Eliminates Pops and Clicks, and Reduces Electromagnetic Interference in Today’s Notebook and Desktop Audio Systems
October 25, 2010
SAN JOSE, Calif., October 25, 2010 – Integrated Device Technology, Inc. (IDT®; NASDAQ: IDTI), the Analog and Digital Company™ delivering essential mixed-signal semiconductor solutions, today announced the world’s first family of high-definition PC audio codecs to feature the DDX™-based class-D modulation technology developed by Apogee Technology. This highly efficient 3-state modulation technique extends battery life, eliminates pops and clicks, and reduces electromagnetic interference (EMI) in notebook and desktop audio systems.
The IDT 92HD9x family of audio codecs integrates equalization, dynamics processing and filtering in hardware to enhance the audio output, complemented by a complete set of features implemented in software to enhance the microphone inputs, such as acoustic echo cancellation, noise suppression and beam forming for unified communications.
“IDT is dedicated to raising the ‘audio bar’ in the computing world,” said Patrick Griffith, senior marketing director of the Analog and Power Division at IDT. “This new family of IDT audio codecs adds to an already comprehensive portfolio and boasts a compelling feature set, allowing customers to select the right codec for a variety of audio configurations.”
The newest audio codecs in the IDT family include an integrated high-pass filter to prevent speaker damage by blocking low frequency content the output transducers cannot reproduce. When used in conjunction with the integrated band-pass filter, 2.1 speaker configurations are possible using the mono subwoofer output.
In addition, the latest members of IDT’s industry leading audio family feature an integrated combo jack, which allows today’s headsets to use a single port for the microphone input and headphone output. This integrated combo jack offers board designers a system-level cost savings by eliminating external components previously needed for microphone detection.
Finally, the 92HD9x family offers an option for dual HD Audio and Inter-IC Sound (I2S) bus interfaces to facilitate notebook docking and the connection of auxiliary audio devices with lower bill of materials costs.
The IDT 92HD91 and 92HD99 are stereo-class class-D codecs available in 48-QFN and 40-QFN packages respectively. The 92HD98 is a mono version of the 92HD99 in the 40-pin QFN package, and the 92HD90 has a feature set similar to the 92HD91 with an added I2S bus interface in 48-QFN. For pricing and other information, please visit www.idt.com/go/audio.
About IDT
Integrated Device Technology, Inc., the Analog and Digital Company™, combines analog and digital technology to develop system-level innovations that optimize customers’ applications and enrich the end-user experience. IDT uses its market leadership in timing, serial switching and interfaces, and adds analog and system expertise to provide complete application-optimized, mixed-signal solutions for the communications, computing and consumer segments. Headquartered in San Jose, Calif., IDT has design, manufacturing and sales facilities throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT is accessible at www.IDT.com. Follow IDT on Twitter and Facebook.
###
DDX™ is a trademark of Apogee Technology, Inc.
IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.