IDT’s PMIC Technology Offers Intelligent, Scalable, Distributed Output Current Capability to Meet Varying SoC Power Requirements and Overcome Thermal Limitations

April 26, 2013

SAN JOSE, Calif., April 26, 2013 – Integrated Device Technology, Inc. (IDT®) (NASDAQ: IDTI), the Analog and Digital Company™ delivering essential mixed-signal semiconductor solutions, today announced the industry’s first intelligent, scalable, distributed power management solution for portable multi-core application processors. IDT’s patented technology offers flexibility to add incremental output current without modifying the controller power management IC (PMIC). This allows the solution to scale with varying system-on-chip (SoC) power requirements and helps to overcome PCB routing and thermal challenges.

          IDT’s innovative technology is a power management solution consisting of a main PMIC with communication lines for the connection and control of IDT’s compact, external, add-on power sources, for increased power output capability. Unlike traditional solutions that require different PMICs for different applications, IDT’s scalable solution minimizes development time and risk with a single PMIC that can be re-used and re-optimized to support the evolving power requirements of various processor platforms. In addition, the distributed nature of the add-on power sources offers tremendous advantages for point-of-load regulation, circuit board routing, and thermal distribution. IDT’s innovative approach is an ideal solution for advanced portable devices, such as tablet PCs, clam shell devices, smartphones, ebooks, high-end digital cameras, client solid-state drives (SSD), and set-top boxes. The IDTP9165 PMIC and IDTP9167 companion power source are IDT’s first devices to offer this technology.

          “IDT’s scalable approach to power management brings a new level of performance and flexibility to the fast-paced market of consumer portable electronics,” said Arman Naghavi, vice president and general manager of the Analog and Power Division at IDT. “When our customers design a new platform of portable devices, it’s difficult to predict exactly how much output power will be needed to optimize each system. As a result, PMICs are typically overdesigned, making the systems costly, inefficient, and physically larger. By providing our customers a flexible power management platform to mirror the needs of their processor platform, they can now focus their attention on a single PMIC, and simply scale the output power to optimize each system. In addition, this modular approach offers invaluable thermal benefits by allowing the designer to spread the power dissipation across the board – a serious challenge in today’s ultra-compact portable devices."

          The IDTP9165 includes five integrated synchronous step-down DC/DC regulators, 11 LDOs, a real time clock (RTC), a 10-bit ADC, multiple GPIOs, and a high-speed I2C interface. The IDTP9167 add-on power sources are controlled by the IDTP9165 PMIC, allowing the designer to command up to eight external devices as though they were integrated into the main PMIC itself. Each optional device efficiently provides up to 6 A of additional peak current, distributing heat across the board and greatly simplifying PCB routing and stack-up requirements near the PMIC – an area that is often a challenge to design. In addition, the transient currents and voltages of the additional phases are contained to the external power sources’ immediate areas, helping to minimize EMI and avoid inductive interference.

          An innovative control system leverages a proprietary two-wire interface without sensitive analog feedback traces or individual pulse width modulation (PWM) line connections. This minimizes the number of PCB traces and avoids potential signal coupling issues, allowing the customer to easily scale the number of add-on power sources required for each application. Furthermore, automatic signal integrity calibration practically eliminates proximity and trace length concerns, allowing customers to separate the host PMIC and power sources as needed to optimize the system.

Availability
          The IDTP9165 PMIC and IDTP9167 scalable power sources are currently being sampled to qualified customers only. Please contact your local sales representative for more information. To learn more about IDT’s multi-channel PMIC solutions, please visit www.idt.com/go/PMIC.

About IDT
          Integrated Device Technology, Inc., the Analog and Digital Company™, develops system-level solutions that optimize its customers’ applications. IDT uses its market leadership in timing, serial switching and interfaces, and adds analog and system expertise to provide complete application-optimized, mixed-signal solutions for the communications, computing and consumer segments. Headquartered in San Jose, Calif., IDT has design, manufacturing, sales facilities and distribution partners throughout the world, with direct purchase services through IDT Direct™. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT is accessible at www.IDT.com. Follow IDT on Facebook, LinkedIn, Twitter, and YouTube.

###

IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.

Share this news on