IDT’s Enhanced 4E MEMS Oscillators Offer Configurable Outputs in an Industry-standard Package Footprint, Saving Board Area in Communication, Networking, and Storage Applications
SAN JOSE, Calif., January 24, 2013 – Integrated Device Technology, Inc. (IDT®) (NASDAQ: IDTI), the Analog and Digital Company™ delivering essential mixed-signal semiconductor solutions, today announced the industry’s first high-performance quad frequency MEMS oscillators with multiple synchronous outputs. IDT’s latest oscillators offer configurable outputs in an industry-standard compatible package footprint, saving board area and bill-of-materials (BOM) cost in communication, networking, storage, industrial, and FPGA applications.
The IDT 4E series ±50 ppm enhanced MEMS oscillators integrate an LVDS or LVPECL output with a synchronous CMOS output into a single package, eliminating the need for an external crystal or secondary oscillator. Available in frequencies up to 600 MHz, the new oscillators save board area, simplify the application circuit, and reduce BOM cost in any high-performance application requiring an LVDS or LVPECL frequency source. Additionally, the oscillators feature two control pins to select between four factory-programmable output frequencies, allowing for the replacement of four components with a single device. This enables the customer to reduce their BOM count, consolidate their inventory, and realize cost benefits.
“Our new CrystalFree™ MEMS oscillators eliminate the need for additional quartz crystals and bring tremendous value to our customers,” said Christian Kermarrec, vice president and general manager of the timing and synchronization division at IDT. “Our new 4E series provides our customers with what they’ve been asking for – simplicity and cost savings. Not only have we met these demands, we’ve also maintained backward compatibility with their existing socket footprints to ease the transition to these new devices.”
The IDT 4E series oscillators are designed with the physical dimensions and pinout of an industry-standard six-pin CMOS, LVDS or LVPECL oscillator, but with four additional pins (10 pins total) strategically placed to maintain backward compatibility with existing six-pin sockets. This allows designers to use the oscillators in existing sockets while offering additional functionality for new designs.
System designers can choose from three different output combinations: LVDS and CMOS outputs, LVPECL and CMOS outputs, or three synchronous CMOS outputs – offering the flexibility to use the innovative devices in a myriad of applications.
Pricing and Availability
The IDT 4E MEMS oscillators are currently sampling to qualified customers and are available in a standard 7.0 x 5.0 mm VFQFPN package. Most standard frequencies are readily available. Custom frequencies can be configured by request. For more information, visit www.idt.com/go/MEMS.
About IDT
Integrated Device Technology, Inc., the Analog and Digital Company™, develops system-level solutions that optimize its customers’ applications. IDT uses its market leadership in timing, serial switching and interfaces, and adds analog and system expertise to provide complete application-optimized, mixed-signal solutions for the communications, computing and consumer segments. Headquartered in San Jose, Calif., IDT has design, manufacturing and sales facilities throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT is accessible at www.IDT.com. Follow IDT on Facebook, LinkedIn, Twitter, and YouTube.
###
IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.