IDT’s Quad-frequency FemtoClock NG Devices Offer Industry-leading Performance as a Highly Flexible Silicon-based Solution for Telecommunication, Computing, Networking and Storage Applications

 
March 6, 2012

SAN JOSE, Calif., March 6, 2012 – Integrated Device Technology, Inc. (IDT®) (NASDAQ: IDTI), the Analog and Digital Company™ delivering essential mixed-signal semiconductor solutions, today announced a new family of quad-frequency programmable clock oscillators leveraging IDT’s fourth-generation FemtoClock® NG technology. The new devices offer industry-leading performance as a highly flexible silicon-based solution for crystal oscillator (XO) and voltage-controlled crystal oscillator (VCSO) replacements.

          The IDT 8N3Q001, 8N4Q001, 8N3QV01 and 8N4QV01 are quad-frequency programmable clock oscillators leveraging IDT’s silicon-based FemtoClock NG technology. They offer excellent high-frequency and low-phase noise performance for demanding telecommunication, computing, networking and storage applications. These devices enable system designers to reduce complexity and cost by replacing up to four XOs with a single IDT quad-frequency clock oscillator. The devices feature programmable output frequencies from 15.476 MHz up to 1,300 MHz, giving engineers the flexibility to reprogram and generate new frequencies without the long delays typically associated with crystal oscillators. IDT’s custom FemtoClock NG products can be received within 6 to 8 weeks on average, instead of the 14 to 16 weeks of typical custom XOs.

          “We’ve built upon our timing leadership to offer a high-performance and highly integrated device to replace outdated fixed-frequency XOs in the $4B frequency control market,” said Fred Zust, vice president and general manager of the Timing and Synchronization Division at IDT. “Our new clock oscillators integrate multiple programmable frequencies into a single package, enabling our customers to simplify their board designs and eliminate the lead-time risks posed by fixed-frequency products in fast-paced design cycles.”

          IDT’s new clock oscillators feature four factory-programmed frequencies that can be customized for different applications and reconfigured by a standard I2C interface. This makes it easy for engineers to reprogram the devices in the lab or on-the-fly in the application. The fourth-generation FemtoClock NG technology operates at phase noise levels below 500 femtoseconds with power supply rejection ratio (PSRR) better than -80 dBc, making it well-suited for high-speed finely tuned systems.

Pricing and Availability
          The IDT8N3Q001, IDT8N4Q001, IDT8N3QV01 and IDT8N4QV01 accept a 2.5 V or 3.3 V power supply and are currently sampling to qualified customers. They are available in a small, Pb-free (RoHS 6) 10-lead ceramic 5 x 7 x 1.55 mm package. For more information about IDT’s frequency control products (FCP), visit www.idt.com/go/FCP.

About IDT
        Integrated Device Technology, Inc., the Analog and Digital Company™, develops system-level solutions that optimize its customers’ applications. IDT uses its market leadership in timing, serial switching and interfaces, and adds analog and system expertise to provide complete application-optimized, mixed-signal solutions for the communications, computing and consumer segments. Headquartered in San Jose, Calif., IDT has design, manufacturing and sales facilities throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT is accessible at www.IDT.com. Follow IDT on FacebookLinkedInTwitter, and YouTube.

 


###

IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners. 

Share this news on

Share this news on