February 19, 2014

TOKYO, Japan, February 19, 2014 — Renesas Electronics Corporation (TSE: 6723) today announced the following changes in its Members of the Board. These changes were approved at the Extraordinary Shareholders’ Meeting and became effective as of today.

Note: Asterisks (*) indicate position currently held.

Newly appointed executives

1. Member of the Board

New Member of the Board

Tetsuro Toyoda
Executive Managing Director, Innovation Network Corporation of Japan *

Retiring Member of the Board

Shigeo Mizugaki
Member of the Board *

Refer to the attachment for a brief biography of the newly appointed Member of the Board and an updated list of Members of the Board and corporate auditors.

Note: Tetsuro Toyoda will serve as an outside Director. Shigeo Mizugaki will assume his position as a Fellow as of February 20, 2014.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.