Renesas Launches Arm Cortex-M33-based RA6M4 MCU Group with Superior Performance and Advanced Security for IoT Applications

Combines Arm TrustZone Technology with Renesas-enhanced Secure Crypto Engine, Octa Memory Interface, and Innovations that Enable Easy Security Solution Designs

06 Oct 2020

TOKYO, Japan ― Renesas Electronics Corporation (TSE:6723), a premier supplier of advanced semiconductor solutions, today announced the expansion of its RA6 Series microcontrollers (MCUs) with nine new RA6M4 Group MCUs, increasing the RA Family to 42 MCUs. These 32-bit MCUs boost operating performance up to 200 MHz using the Arm® Cortex®-M33 core based on Armv8-M architecture with Arm TrustZone® technology. The RA6M4 MCUs deliver optimized performance together with leading-edge security and connectivity supported by the easy-to-use Flexible Software Package (FSP). In addition, the Renesas partner ecosystem offers software and hardware building blocks that work out-of-the-box with RA6M4 MCUs and FSP to address Industrial 4.0, building automation, metering, healthcare, and home appliance applications.

With strong security, rich connectivity, large embedded RAM with parity/ECC, low power consumption, and leverage of the Arm developer and tools ecosystem, the RA6M4 MCUs speed the development of intelligent IoT edge and endpoint devices. Renesas’ enhanced Secure Crypto Engine delivers excellent security solutions, incorporating multiple symmetric and asymmetric cryptography accelerators, advanced key management, security lifecycle management, tamper detection, and increased resistance to side-channel attack, in addition to Arm TrustZone technology. These integrated security features make the RA6M4 MCUs the ideal choice for connected applications, and enable customers to realize lower BOM cost and secure element functionality in all their IoT designs.

“Delivering on our promise at the launch of the RA MCU Family last October, I’m proud to announce its expansion with the RA6M4 MCUs. They offer customers best-in-class performance and security enhancements built with Arm Cortex-M33 cores that clearly deliver more memory, memory interface expansion, better power efficiency and wake-up time, and more connectivity options,” said Roger Wendelken, Senior Vice President of Renesas’ IoT and Infrastructure Business Unit. “We intend to delight our customers who appreciate the higher level of security and IoT connectivity that the RA6M4 MCU Group brings with the confidence and ease of use that only comes by designing with Arm and securing with Arm TrustZone technology.”

“IoT edge and endpoint technologies are opening up new opportunities for developers to build smaller devices, with greater privacy and less dependence on the cloud,” said Dipti Vachani, senior vice president and general manager, Automotive and IoT Line of Business at Arm. “The RA6M4 MCUs move intelligence closer to the data, with Arm TrustZone technology built in to ensure privacy and data integrity, helping securely accelerate the growth of IoT.”

Built on a highly efficient 40nm process, the RA6M4 MCUs drive power consumption down to 99uA/MHz while running the CoreMark algorithm from flash. The MCUs also support fast wakeup times of 30 µs from standby using a high-performance on-chip oscillator. Their high integration up to 1MB code flash memory and 256 KB of SRAM (64 KB with ECC) also make the RA6M4 MCUs well suited for low power and safety applications.

Key Features of the RA6M4 Group

  • 200 MHz Arm Cortex-M33 with TrustZone technology
  • Renesas’ Secure Crypto Engine as part of a full security solution
  • Scalable from 64-pin to 144-pin LQFP packages
  • Ethernet controller with DMA
  • Capacitive touch sensing unit
  • USB 2.0 Full Speed and CAN
  • QuadSPI and OctaSPI memory interface, and advanced analog
  • SCI (UART, Simple SPI, Simple I2C), and SPI/ I2C multimaster interface
  • SDHI and SSI (Serial Sound Interface)

The RA6M4 with Flexible Software Package (FSP) allows customers to re-use their legacy code and combine it with software from partners across the vast Arm ecosystem to speed implementation of complex connectivity and security functions. The FSP includes FreeRTOS and middleware, offering a premium device-to-cloud option for developers. These out-of-box options can be easily replaced and expanded with any other RTOS or middleware.

The FSP provides a host of efficiency enhancing tools for developing projects targeting the RA6M4 MCUs. The e2 studio Integrated Development Environment provides a familiar development cockpit from which the key steps of project creation, module selection and configuration, code development, code generation, and debugging are all managed. FSP uses a GUI to simplify the process and dramatically accelerate the development process.

Availability

The RA6M4 MCUs are available now from Renesas’ worldwide distributors. For more information, please visit: www.renesas.com/products/microcontrollers-microprocessors/ra/ra6/ra6m4.html.

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power, and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, and YouTube.

(Remarks). Arm, Arm Cortex, and Arm TrustZone are trademarks or registered trademarks of Arm Limited in the EU and other countries. CoreMark is a registered trademark of the Embedded Microprocessor Benchmark Consortium. All names of products or services mentioned in this press release are trademarks or registered trademarks of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.