Renesas Selects Andes RISC-V 32-Bit CPU Cores for its First RISC-V Implementation of ASSPs

01 Oct 2020

TOKYO, Japan ― Renesas Electronics Corporation (TSE:6723), a premier supplier of advanced semiconductor solutions, today announced a technology IP cooperation with Andes Technology, an advanced supplier of RISC-V based embedded CPU cores and associated SoC development environment. Renesas selected the AndesCore™ IP 32-bit RISC-V CPU cores to embed into its new application-specific standard products that will begin customer sampling in the second half of 2021.

“We are thrilled that Renesas, a top-tier global MCU provider has designed Andes RISC-V cores into their pre-programmed application-specific standard products. Renesas and Andes share the same vision to welcome the era of RISC-V being the mainstream CPU instruction set architecture (ISA) for system-on-chips (SoC),” said Frankwell Lin, President of Andes Technology Corp. “Not only does this represent a milestone for Andes, but it marks the arrival of the open-source RISC-V ISA as a mainstream computing engine. Renesas customers will benefit from a modern ISA constructed for the needs of 21st century computing.”

“The scalable range of performance, selectable safety features, and customization options provided by the Andes RISC-V core IP enables Renesas to provide innovative solutions for future application-specific standard products,” said Sailesh Chittipeddi, Executive Vice President, General Manager of Renesas’ IoT and Infrastructure Business Unit. “Customers looking for cost-effective alternative paths for existing or emerging applications will benefit from the reduced time to market and lower development costs.”

The delivery of Renesas’ pre-programmed ASSP devices based on the RISC-V core architecture, combined with specialized user interface tools to set the application programmable parameters, will provide customers with complete and optimized solutions. This capability eliminates the initial RISC-V development and software investment barrier. In addition, an extensive network of regional Renesas partners with specialized expertise will provide cutting edge and sharply focused customer support.

About Andes Technology

Andes Technology Corporation is a world-class creator of innovative high-performance/low-power 32/64-bit processor cores and associated development environment to serve the rapidly growing global embedded system applications. The company delivers superior low power CPU cores, including the comprehensive RISC-V V5 family of processor IPs, with integrated development environment and associated software/hardware solutions for efficient SoC design. Up to the end of 2019, the cumulative volume of Andes-Embedded™ SoCs has surpassed the 5-billion mark. Andes Technology's comprehensive CPU line includes extensible entry-level, mid-range and high-end families. For more information, please visit http://www.andestech.com.

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power, and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, and YouTube.

(Remarks) All names of products or services mentioned in this press release are trademarks or registered trademarks of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.