Renesas Electronics New R-Car V2H Device Offers High-Resolution Image Recognition for Safer Driver Assistance Systems in Conventional and Emerging Self-Driving Vehicles

Single-Chip Device Packs Company's Ground-Breaking Image Recognition Technology and Other Functions for High-Performance, Low Power, and Improved Safety

28 Aug 2014

TOKYO, Japan, August 28, 2014 — Renesas Electronics Corporation (TSE: 6723), today announced the availability of its R-Car V2H, the company's newest system-on-a-chip (SoC) implementing state-of-the-art image recognition technology to support high-resolution surround viewing in advanced driver assistance systems (ADAS). This is the first R-Car ADAS device from Renesas and includes additional functionality for higher performance, lower power, and improved safety in traditional and emerging self-driving vehicles.

Renesas applied technology from its industry-leading R-Car SoCs for automotive infotainment equipment and added high-performance image recognition and low-power consumption technologies in the development of the R-Car V2H. The R-Car V2H enables embedded system manufacturers to deliver high-resolution surround-view monitoring systems, with multiple cameras, for advanced point-of-view switching. This includes rear-view and surround-view capabilities that expand what is seen by the system to every direction around the vehicle, aiding in driver oversight prevention. These types of sophisticated systems demand substantially higher processing performance in order to handle the expanded range of image recognition targets and increased processing load imposed by multiple cameras with higher pixel counts. At the same time, there is demand for both functional safety, to maintain high quality and performance, and reduced power consumption. Finally, the rapidly increasing cost of software development creates a need for better development efficiency. The Renesas R-Car V2H addresses all of these requirements in a single-chip solution.

“As a premier supplier of advanced semiconductor solutions to the automotive industry, Renesas is mindful not only of the electronic system requirements of today and tomorrow's automobiles, but also the importance of safety, especially with wider adoption of self-driving vehicles,” said Ryuji Omura, Executive Vice President at Renesas Electronics Corporation. “The R-Car V2H series delivers the imaging technologies, software tools, and high-speed networking needed to develop robust ADAS systems that contribute to smarter, safer automobiles.”

Key Features of the R-Car V2H SoC:

  • (1) Integration of essential ADAS functions on a single chip and low power consumption

The R-Car V2H SoC incorporates the IMR, a core dedicated to viewpoint conversion, the Renesas IMP-X4 image recognition core, and a 3-D graphics core, all of which provide the imaging-related technologies needed to support ADAS requirements on vehicles targeting new government regulations and insurance safety ratings. The overall architecture of the R-Car V2H is optimized in order to reduce memory bandwidth usage and overall latency. Six IMR channels can each support a high-resolution camera where the combined output can produce high-definition surround view images. The IMP-X4, in combination with the CPU, offers high performance for real-time processing of image data as it is captured from the camera. The 3-D graphics core enables a human-machine interface (HMI) that can deliver high visibility and easy identification of hazards and is optimized to support texture mapping from the camera feeds. While integrating the above functionality on a single chip, the R-Car V2H device also incorporates functions to reduce power consumption to the levels required by automotive systems. This includes a system design that balances performance and power consumption, a power cutoff function for the integrated cores, and a DDR3-SDRAM power backup function.

 

  • (2) Expansion of image recognition library support to include an open source library (OpenCV, Note 1) for improved software development efficiency

The IMP-X4 image recognition core delivers image recognition processing performance that is approximately eight times that of the earlier Renesas SH7766 and approximately four times that of the R-Car H1. The IMP-X4 incorporates six programmable image processing accelerators making possible image recognition functionality involving, for example, processing of input from multiple cameras, while altering their configuration as needed.


The Renesas exclusive image recognition library support has been expanded to include an open source library (OpenCV), substantially increasing the efficiency of software development for the customer. The image recognition library does not require fine tuning to extract full performance from the image recognition core, delivering consistently stable performance and allowing for smooth software upgrades. In addition, the library is backward compatible with the IMP series employed in the earlier R-Car H1 and SH7766 Renesas products, making it easy to reuse existing software resources.

 

  • (3) Ethernet AVB in combination with optimized video codecs for next-generation automotive networks and camera systems

Ethernet AVB offers features such as guaranteed bandwidth and synchronization of multiple cameras. Moving forward, it is expected to become the mainstream technology for automotive high-speed networking. The R-CAR V2H includes a gigabit Ethernet AVB controller to work with next-generation automotive networks.


In combination of the introduction of the Ethernet AVB technology with optimized features for multiple-camera reception, Renesas also integrated multiple-channel video codecs supporting up to 5 high resolution cameras in parallel. In order to support technical transition processing of video codecs for surround view monitoring systems, R-Car V2H supports MJPEG & H.264.

Based on long experience in functional safety for embedded systems, the R-Car V2H has been designed to achieve high level functional safety. For example, ECC has been implemented on external memory and CPU caches in order to support system manufacturers' safety concepts. Additionally, the hardware CRC functionality makes it easy to achieve end-to-end protection of data transfers. In addition, the early adoption of the highly reliable INTEGRITY® real-time OS from Green Hills Software is an important step toward achieving functional safety in both hardware and software.

 

“Our partnership with Renesas has allowed us to develop an innovative solution for the new revolutionary R-Car V2H ADAS platform,” said Tim Reed, vice-president of advanced products at Green Hills Software. “By introducing the industry's most trusted real-time operating system-INTEGRITY-and its award winning security and functional safety architecture, Renesas has created an offering that delivers guaranteed real-time determinism and safety to its customers. When I go out and buy a new automobile in the future, I will drive easier knowing that this platform is riding alongside me, guiding my car, and helping me and other drivers stay safe.”

Refer to the separate sheet for the main specifications of the R-Car V2H SoC.

Availability

Samples of the R-Car V2H SoC will be available in September 2014. Mass production is scheduled to begin in October 2016, and is expected to reach a combined production volume of 500,000 units per month by October 2017.

 

For more product information, please visit: https://www.renesas.com/en/solutions/automotive/soc/r-car-v2h.html

(Note 1) OpenCV (Open Source Computer Vision

An open source computer vision and machine learning software library. This wide-ranging library can be used free of charge, and it has been widely adopted for the development of image recognition programs on the PC.

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power, and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, home electronics, office automation, and information communication technology applications that help shape a limitless future. Learn more at renesas.com.

(Remarks) INTEGRITY is a trademark or registered trademark of Green Hills Software, Inc., in the United States of America and other countries. All other names of products or services mentioned in this press release are trademarks or registered trademarks of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.