TES Guiliani Graphical User Interface on RZ/A Stream it! - RZ - V2.0!
跳转至页面部分:arrow_drop_down
2018-10-25
Welcome to this demonstration of TES Guiliani on Renesas new solution kit Stream it! - RZ-V2.0. The Stream it! - RZ-V2.0 is based on RZ/A1-LU MPU, which runs at 400MHZ, provides 3MB of embedded SRAM and is optimized for HMIs from the ground up.