2018-06-22

Renesas is the first major MCU supplier to provide a bundled, commercially-available, and qualified software package that is specifically developed and optimized for a family of scalable MCUs. Embedded system developers can use the Renesas Synergy™ Software to immediately begin writing their application code at the API level. The Synergy Software Package (SSP), a vital component of Renesas Synergy Software, is warranted by Renesas to operate within the specifications published in the software datasheet. The ability to start writing code at the API level is redefining how embedded systems and IoT products will be developed and maintained over their product life cycles. In the past, software for MCU has been provided by MCU suppliers on an "as is" basis with no warranty, no systematic long-term maintenance, and without a complete package that included a major commercial RTOS at its core. The Synergy Software eliminates all these deficiencies and is the heart of the Renesas Synergy Platform. Watch the video to learn more.