下载 (D4000382)

发布日期 : Apr.05.17

类别 : Evaluation Software, IDE Upgrades

e² studio 5.4 installer (Web installer)

Description

  • Click below for detailed information.

    This installer requires the Internet connections.
    "Offline Installer" available from here is capable of installation under offline environment.

 

How to install

Please download the installer file from the "Download Link" shown below, then launch the installer.

Note 1: e² studio has no capability to update from V3.x, V4.x or earlier versions to V5.0 or later including V5.4.
“Update” installation should not be applied to V4.x or earlier installation folder.
Please uninstall the earlier versions before installation.
Alternatively, if you would like to keep an earlier installations, please create a new folder for the new installation.
Note 2: Windows OS may display a warning message "This program might not have installed correctly" after installations have done. This message does not mean installation failure. Please dismiss the message box by choosing "This program installed correctly".
Note 3: Before launch install or update, please close all projects in the current workspace. (Choose "Close Project" in the "Project" menu.)
Installation process can be interrupted by the opened projects.

 

Operating Environment

  • Windows® 10 (32-bit, 64-bit)
  • Windows® 8.1 (32-bit, 64-bit)
  • Windows® 7 (32-bit, 64-bit)

下载

产品名称 文档 名称 文档 大小 下载链接
e² studio 5.4 installer (Web installer) setup_e2_studio_5_4_web.exe 82.12 MByte