The Renesas integrated development environment, or the High-performance Embedded Workshop, supports Tcl/Tk Version 8.4.4. Tcl/Tk is comprised of a class member "Tcl" of script language (Tool Command Language) and the "Tk" (Tool Kit) used to program a graphical user interface. Use of Tcl/Tk helps to create appropriate GUIs that suit the development environment, in addition to the functions and GUIs supplied by the High-performance Embedded Workshop, thereby extending the development environment further.
|
|
|
---|---|---|
类型 | 文档标题 | 日期 |
Release Note | PDF 307 KB 日文 | |
手册 - 开发工具 | PDF 4.16 MB 日文 | |
手册 - 开发工具 | PDF 1.85 MB 日文 | |
应用文档 | PDF 1.43 MB | |
4 items
|
The High-performance Embedded Workshop offers a Console window that supports Tcl/Tk programming and a GUI window.
The Console window of the High-performance Embedded Workshop permits Tcl/Tk programming to be performed in interpreter mode or script file load mode.
During programming with Tcl/Tk, various commands supported in the High-performance Embedded Workshop environment can be used. By using Tcl/Tk and these commands in combination, it is possible to create GUIs that control the High-performance Embedded Workshop environment.
The usable commands of the High-performance Embedded Workshop differ with the target MCU for which the simulator and emulator are used. For details on how to use, refer to Tcl/Tk Application Notes.
Basic Tcl/Tk sample programs are supplied from Renesas. Use these samples to understand the basic method of programming.