概览

简介

GR-PEACH is the Gadget Renesas board for the Renesas RZ family's RZ/A1H group of microprocessors (MPU) products. Fully pin-compatible with Arduino UNO, GR-PEACH is an Arm® MbedTM enabled development platform. GR-PEACH takes advantage of web browser-based program development and a robust library selection. With the added appeal of 10MB of built-in RAM and the processing power of Arm CortexTM-A, GR-PEACH was created for the developer interested in high-speed prototyping of IoT devices with loads of HMI—graphics, touch panel, camera input, audio, network and more.

In addition, RZ/A1H FreeRTOSTM Software Package for GR-PEACH has been released.

peach-position-chart
logo-arm-mbed
microsoft-azure-logo

In addition, GR-PEACH supports multiple platforms, .NET Micro Framework (MF), Arduino, and TOPPERS/ASP (RTOS). Click the platform figures below to be directed to the respective getting started pages.

peach-multi-mbed
peach-multi-netmf
peach-multi-arduino
peach-multi-toppers

Key Features

GR-PEACH Board

Embeds Arm Cortex-A RZ/A1H (R7S721001VCBG) and Arduino UNO pin compatibility supports various shields.
Corestaff vendor's site

gr-peach-board

GR-PEACH-FULL Board

GR-PEACH board is equipped with a LAN connector (RJ-45) and connectors for Arduino UNO compatible pins and service pins.
Corestaff vendor's site

gr-peach-full-board

GR-PEACH Wireless Camera Shield

Enables camera and Wi-Fi connection with the GR-PEACH board. Camera specifications are VGA 640 x 480, maximum 60fps and a horizontal angle view of 98 degrees.
Corestaff vendor's site

gr-peach-wireless-camera

GR-PEACH Audio Camera Shield

Enables stereo plug, camera module and USB host connection with GR-PEACH.
Note: A camera module is not included. MT9V111 is recommended.

gr-peach-audio-camera

GR-PEACH 4.3-inch LCD Shield

4.3-inch wide display with touch panel.
Note: GR-PEACH-FULL cannot be used for this shield. Refer to the vendor's site for the use detail.
Corestaff vendor's site

gr-peach-lcd

Certification

CE, EU RoHS, China RoHS

 

GR-PEACH Pin Map

The pin map below is for sketching with Arduino style on the Renesas web compiler. If the Mbed development environment is being used, visit the Mbed site.

gr-peach-pin-map

Detailed Specification

Microcontroller
RZ/A1H (R7S721001VCBG 324-pin BGA)
ROM/RAM
External FLASH 8MB/Internal 10MB
Operating Frequency
400MHz
Operating Voltage
3.3V/1.18V
Board Function
USB host/peripheral (exclusive selection), Ethernet, XBee interface, Micro SD socket, JTAG interface, user switch, reset switch, Arduino shield interface, user LEDs, USB mass storage class-like programming.

应用

文档

类型 文档标题 日期
Release Note 登录后下载 PDF 217 KB
1 item

设计和开发

样例程序

Resources


Project File for e2 studio

Project file for sketching in Eclipse-based development environment e2 studio. For downloading and installing e2 studio, please refer to the e2 studio product page.

You can import as an archive file (zip) as an existing workspace from the e2 studio menu "File" -> "Import".

Do the menu "Project" -> "Update all dependencies" at the initial build. Only sources changed since the next build will be compiled.

DisplayApp

DisplayApp is an application that displays the camera image sent by USB CDC.

Installing the USB driver is required on versions earlier than Windows 10.

Below is an Arduino-like sketch example.

    
    #include <Arduino.h>
    #include <Camera.h>
    #include "DisplayApp.h"
    Camera camera;
    static DisplayApp display_app;
    void setup() {
        camera.begin();
    }
     
    void loop() {
        display_app.SendJpeg(camera.getJpegAdr(), (int)camera.createJpeg());
        delay(10);
    }
    }
    

Projects

Gadget Renesas provides boards that make it possible to prototype ideas quickly, a community where users can interact, and events to help users build their projects to make their ideas a reality. Below are some projects that utilized the GR-PEACH board.