图像
船橋 豊
Yutaka Funabashi
Principal Software Engineer
已发布: 2022年5月25日

Issues in the Development of Evolving E/E Architecture

Figure 1 shows the issues of the E/E architecture. Due to the huge amount of complicated processing required in next-generation vehicles, many ECUs shall be installed, and the system scale and software are increasing.

图像
E/Eアーキテクチャの課題

 

Figure 1. The issues of the E/E architecture

Figure 2 shows changes in the scale of in-vehicle software.
Software processing is increasing in size and complexity.
This leads to a significant increase in the importance of software, development periods and man-hours.

图像
Fig2-a Smartphone / Car comparison
图像
Fig2-b Graph

Figure 2. Changes in the scale of in-vehicle software

On the other hand, to enhance the value of vehicles, it is necessary to develop reliable software in a shorter cycle, so new development methods and development environments should be introduced.

Overview of Virtual Turnkey Platform

To solve the above problems, Renesas provides the Virtual Turnkey Platform that allows you to start software development without an actual device. By providing a Virtual Platform (VPF) that simulates the operation of the entire actual device and a Software Development Kit (SDK) that runs on the VPF, customers can start software development before obtaining the actual device. Since the software developed on VPF works on the actual device, it is possible to develop and verify the software on the actual device without delay after obtaining the actual device.

Figure 3 shows an example related to the R-Car S4 Virtual Turnkey Platform, which is indicated by the red dotted line in the figure.

图像
R-CarS4のVirtual Turnkey Platform具体例

Figure 3. An example of the R-Car S4 Virtual Turnkey Platform

R-Car S4 has the function of a communication gateway and is connected to the blocks for sensing, cognitive, cockpit, and various controls, which communicate with each other. Virtual Turnkey Platform consists of the R-Car S4 VPF, routing accelerator software that controls the Ethernet switch in R-Car S4, MCAL driver that controls communication, and so on. Customers can develop communication gateway application software by using the software provided by Renesas (Software Development Kit (SDK)).

Normally, when customers develop software, it is necessary to prepare hardware equipment and debugging tools, such as an evaluation board and an emulator. But, it takes much time to prepare. Instead, Virtual Turnkey Platform enables customers to start software development easily by the following two processes.

  • Install the VPF provided by the tool vendor on your PC.
  • Download the corresponding SDK from the Renesas homepage (R-Car Market Place) with a one-click license.

In this way, customers can easily start developing application software by obtaining the Virtual Turnkey Platform.

Development Status of R-Car Virtual Turnkey Platform

This time, we have released the R-Car S4 Virtual Turnkey Platform to our customers. In the future, we will prepare the Virtual Turnkey Platform for R-Car V4H and Gen 5, the next-generation R-Car series so that customers can accelerate their software development and system consideration.