2015年2月18日

Dusseldorf, February 18, 2015 — Renesas Electronics Europe, a premier supplier of advanced semiconductor solutions, today announced the availability of its new Detect it! solution kit. The Detect it! is designed for detector applications and provides ready to use demonstrators for the most typical detectors used in security and fire protection systems. Detect it! has four hardware boards, a motion detector demonstrator, a smoke detector demonstrator, a carbon monoxide demonstrator, and a glass-break detector demonstrator.

The new solution kit provides a complete solution platform for Renesas’ new RL78/I1D microcontroller group. The RL78/I1D devices offer a comprehensive set of analogue features. The small 48-pin package includes 4 operational amplifiers, 2 comparators and 17 input channels for the 12-bit ADC converter. The RL78/I1D has smart peripherals that are able to work without CPU intervention and in low power modes offer a significant power saving. The smart peripherals can transfer data, compare data, perform addition and subtraction and link one peripherals operation to another peripheral. This offers new possibilities to developers of detector applications. Power consumption has also been further reduced compared to previous generations, achieving 124µA @1 MHz in operation. Fast wake-up time reduces power consumption even more and enables the device to react faster, this is especially beneficial for communication protocols.

Each of the boards provides a solution for the associated detectors. The smoke detector senses smoky environments by the scattering of the infrared signal in a smoke chamber. Motion is detected using PIR technology. The glass-break detector analyses sounds and can differentiate window-break sounds from the surrounding environment. The carbon monoxide detector uses a chemical sensor to measure the concentration of the gas in the surrounding air and generates an alert if the levels are dangerously high. The documentation provided within the kit guides the user and explains the board behaviour in detail.

The Detect it! kit is ready for use out of the box. Users simply choose the board and insert a battery (included in the kit), follow the quick start guide and can get a detector working in less than one minute. The kit provides a good starting point to the developer as it includes the source code of the demonstration sample programs, the environment development installer of IAR Embedded Workbench, the Gerber files and the schematics, and a comprehensive user manual. As this kit was specifically designed for detectors, it brings significant time- and cost-saving advantages to both new and established developers in this field.

About Renesas Electronics Europe

Renesas delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live – securely and safely. As the number one global supplier of microcontrollers, and a leader in A&P and SoC products, Renesas provides the expertise, quality, and comprehensive solutions for a broad range of Automotive, Industrial, Home Electronics (HE), Office Automation (OA) and Information Communication Technology (ICT) applications to help shape a limitless future.

Renesas Electronics Corporation was established in 2010 and is headquartered in Japan.With over 800 hardware and software alliance partners worldwide, it has the industry’s largest local support network. Renesas Electronics’ European structure is comprised of three business units – the Automotive, the Broad-based and the Industrial Solution Business Unit.

Further information about Renesas Electronics Europe is available at www.renesas.com

Renesas Electronics Europe is also on social media at http://twitter.com/Renesas_Europe, http://facebook.com/RenesasEurope and http://youtube.com/RenesasPresents.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.