2013年2月14日

TOKYO, Japan, 14th February, 2013 — Renesas Mobile Corporation, a leading supplier of advanced cellular semiconductor solutions and platforms, today announced the SP2532, the third generation of its GSM/HSPA+/LTE FDD/ LTE TDD multi-mode modems. Supporting full LTE Category 4 (Cat-4) capabilities 150Mbits download and 50Mbits upload combined with the industry's lowest LTE power consumption results in greater speed with enhanced battery life. Coupled with a very small footprint 45% smaller than the previous generation SP2531, very low power consumption and high levels of integration it offers OEMs a fast track to device deployment reducing R&D effort and risks.

“This next generation slim modem platforms, the SP2532 will allow OEMs to design compelling mobile devices which take advantage of lightening quick throughput and low latency for interactive games, rapid web browsing and video streaming and data-rich enterprise application.”, commented Heikki Tenhunen, Senior Vice President Renesas Mobile Corporation. “In addition to enabling exciting new use cases at the lowest power possible, the small chipset footprint also offers the possibility to create new form factors and supports all key operator requirements for 2013 and 20141 including VoLTE, SRVCC and OTDOA.”

The SP2532 delivers high speed broadband on the go, and is able to deliver sustained Cat-4 throughputs of 150Mbits download and 50Mbits upload for both smartphones and data centric devices such as mobile tablets or dongles. Using Cat-4 in a 20MHz bandwidth the SP2532 can achieve 20% more efficient power consumption than leading competitive products, requiring a meager 2mA per Mbit. This impressive performance enhances battery life for example when downloading large files such as videos, music and browsing complex webpages enabling users to stay connected for longer on a battery charge.

Designed with flexibility and choice in mind for the customer, the SP2532 is compatible, and has been pre-integrated with, all the currently available open market application processors. This enables customers to leverage their existing software and hardware assets while upgrading to LTE or to select the most appropriate processor to meet the requirements of new devices. The product also inherits the maturity of previous generations' extensive certification and testing on worldwide networks. OEM customers not only enjoy the peace of mind associated with a proven thoroughbred modem, but also reduce product development and device certification schedules.

The SP2532 comprises a highly integrated baseband modem, an RF subsystem containing the RF integrated chip, front end module, a power amplifier and a power management sub-system. It is available to OEMs today for design-in.

1 Examples include VoLTE and Emergency Calls over LTE, OTDOA & eCellID for SUPLv2, Intra, Inter SON (self organising networks)/ANR (Automatic Neighbor Relations) and CMAS

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, and YouTube.

(Remarks)
All product names and service names that appear in this press release are all trademarks or registered trademarks of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.