RZ/Gプラットフォームでの製品開発に役立つ情報をご提供しております
CIP

RZ/G Linux Platformは、CIPプロジェクトが提供する、10年を超える長期サポートLinuxカーネルを採用しています!Linuxカーネルのメンテナンスに費やすコストを削減でき、信頼性の高い産業グレードのLinuxカーネルを製品に導入することができます。
ルネサスエレクトロニクス株式会社
ソリューション事例(デモ動画)
RZ/GによるEtherCAT通信制御デモ
ルネサス エレクトロニクス株式会社
ヒューマンマシンインタフェース(HMI)に適したRZ/Gシリーズ、モータ制御に適したRZ/Tシリーズ、そしてハードウェアアクセラレータR-INを組合せたGUI操作ができる高度なモータ制御デモセットです。
RZ/G~危険を検知するステレオカメラ
ルネサス エレクトロニクス株式会社
物体認識技術を応用した危険感知システムのデモです。
ステレオカメラの3D処理情報による秒間10コマの物体認識処理をRZ/Gで行います。空港や駅などの社会インフラにてステレオカメラが自律的に危険感知する様子がご覧になれます。

MIRACLE Secure OTA IoT向けセキュアOTA
ミラクル・リナックス株式会社
RZ/Gで利用できるセキュアなデータ展開とアップデートを実現するクラウドシステムです。
MIRACLE Secure OTAでは様々な証明書を利用して、開発者とデバイスを相互認証し、不正なソフトウェアがIoTデバイスに入り込むのを防ぎます。RZ/Gの場合セキュリティ領域TSIPに製品証明書が格納され外部から証明書を操作することができないため、証明書の安全性も担保されます。微細なコンテンツの修正から、ファームウェアやOSレベルのメジャーバージョンアップまで幅広く対応することが可能です。
すぐにアプリケーション開発が可能 EtherCAT開発の為のソフトウェア
JSLテクノロジー株式会社
EtherCATのマスターとスレーブ用のSDKを紹介するデモです。
RZ/G1Eにマスター用acontis社(ドイツ)のSDK実装、R-IN32、EC-1、RZ/T1にスレーブ用SLテクノロジー社製のSDKを実装しています。JSLテクノロジーの充実したサポートによりスムーズな製品開発が可能です。

Renesas RZ/G Door Phone Demo
Renesas Electronics Corporation
This is the Renesas RZ/G1 video door-phone demo in which one live video signal and three H.264-compressed MP4 movies are sent over Ethernet between sending and receiving boards (in this case RZ/G1M Starter Kits). This demo showcases multi-stream video compression/decompression along with Qt graphics.

Renesas RZ/G Qt and Multimedia Demo
Renesas Electronics Corporation
The Linux BSP provided with the RZ/G Development kits contains a number of demos that can be launched from the Linux desktop. These include several demos that come with the Qt framework – for instance: Qt everywhere, Qt cinematic experience, as well as numerous Qml video shader effects.

Renesas RZ/G Embedded Vision Object Recognition Demo
Renesas Electronics Corporation
This is an example of a computer vision application that demonstrates object identification on the RZ/G1M microprocessor. It was developed by Renesas software partner, Uncanny Vision, and uses the Caffe deep learning framework and a convolutional neural network (CNN) - called the Uncanny DLL (Deep Learning Network) - to perform the object identification.
Renesas RZ/G and Crank Software Demo
Renesas has partnered with GUI tool developer, Crank Software, for both the RZ/A and RZ/G Series of MPUs.In this multi-application demo, created with the Crank Software Storyboard Suite and running on the RZ/G1M MPU,we demonstrate sample UIs for home or industrial thermostat, security panels, and building automation.
Renesas Electronics Corporation
Solution Partners

Industrial Surveillance Camera
Industrial Surveillance camera is a 1080p CMOS camera based on Renesas R8A77450(RZ/G1E) Processor with IR LEDs and night vision capability. It contains one main camera and there is a provision for secondary AHD camera on board, which user can add if required. Surveillance camera captures the video and stream it over Ethernet/ 4G LTE/ Wi-Fi networks.
VVDN Technologies Pvt Ltd

マルチプラットフォーム対応の1500を超える豊富なC++ライブラリにより、高い生産性で洗練されたGUIやタッチ操作を実現可能な開発フレームワークです。
株式会社SRA
Arm®認定テクニカルトレーニング(Arm Approved Training Center)
Arm組込み開発が初めての方から、開発の第一線で活躍されているエンジニアの皆様まで、幅広くご満足いただける多種多様なトレーニングコースを用意
株式会社DTSインサイト

Real-Time Capable Virtualization Solutions
In the course of the more and more increasing amount of CPU cores on modern embedded systems, virtualization becomes an important issue in current and future projects. Jailhouse offers Real-Time Capable Virtualization Solutions.
emtrion GmbH

Support, maintenance, customizations, optimizations, and BSP development for a Linux distribution require expertise and a substantial commitment of time and efforts throughout the product life cycle.
ENEA

In general Codethink provide:
- Software engineering to deliver hard, system level projects
- World class Linux and Open Source expertise
- Solution and architecture design
- Consultancy to improve software engineering practice
- Design and build of software engineering tools
- Strategies for long term maintenance of software
- Lower client dependence on software vendors and third parties
- Leveraging open source software and practice
- Leveraging automation
KritiKal Solutions Pvt. Ltd.

Your Innovation Partner – Product Engineering Services in Embedded Vision and AI
KritiKal Solutions is a technology design house specializing in Outsourced Product development and R&D.
KritiKal Solutions Pvt. Ltd.
~産業機器の長期運用と産業グレード (堅牢性・セキュア・信頼性・リアルタイム性能)に対応~ 組込みLinux プロフェッショナルサービス
インダストリアルネットワーク向けマイコン「RZ/Gファミリ」を使った製品開発を包括支援する、組込みLinuxプロフェッショナルサービスのご提供
株式会社大阪エヌデーエス