High-Reliability PLC Solutions
Renesas Electronics Corporation
This is a demo of Renesas’s high-reliability power line communication (PLC). It is widely recognized as a “connected PLC” that is highly resistant to noise, and is even used as the standard at the G3-PLC standards conformity tests. We also have flexible PLC platforms that can provide an optimal environment across all use cases regardless of voltage type (AC/DC).
This video explores uses for the system in disaster prevention systems and building automation.