Smart infrastructure realized by “e-AI” ~ structure monitoring, diagnosis of potential abnormality for structure

Renesas Electronics Corporation

We, Renesas offer the embedded AI (e-AI) which has “Digital Curation”, “Data capture” and “Judgment” to make best performance for a system. The entire system optimization can be realized by respective autonomous actions of edge device, gateway and cloud service. Furthermore, addition or change of all sensors is supported flexibility according to user’s purpose by the platformed edge device.
The following video shows an example of demo where structures such as buildings are analyzed/diagnosed to check a potential abnormality with vibration sensors mounted on the edge device.

Added on 2018-05-11