SAN JOSE, Calif., June 30, 2008 – IDT® (Integrated Device Technology, Inc.; NASDAQ: IDTI), a leading provider of essential mixed signal semiconductor solutions that enrich the digital media experience, today announced a family of ultra-low-power timing devices designed for use in ultra-mobile PCs (UMPCs). These ultra-low-power timing devices minimally require 1.5 volt power supply, as opposed to the 3.3 volts for standard timing devices, helping extend the battery life of the UMPC.
The IDT UMPC timing devices also help extend the wireless signal range of the UMPC and improve the bandwidth, resulting in faster data transfer rates and improving the end user’s mobile Internet experience. They do this by supporting spread spectrum for reducing electromagnetic interference (EMI) and supporting programmable slew rate for reducing radio frequency interference (RFI).
IDT Timing Devices Reduce Interference, Increasing Bandwidth and Data Rates
June 30, 2008
“Our UMPC timing devices continue the IDT focus on power optimization, helping our customers extend the battery life of their products,” said Eric Leung, vice president and general manager of the IDT PC Clock division. “IDT also plays a key role in enhancing the digital media experience, and our UMPC timing devices are customized to help increase system bandwidth, making your mobile Internet experience more enjoyable.”
Features and Benefits
The IDT UMPC timing devices feature a 6mm by 6mm micro lead frame (MLF) package, making it 56 percent smaller than standard 8mm by 8mm packages, offering IDT customers a significantly reduced footprint on the board, thus reducing the overall size of the UMPC.
IDT also features pin-compatible UMPC timing devices for automotive and industrial applications. These devices are designed for use in applications, such as automotive infotainment, embedded and automation systems, that require an industrial operating temperature range (-40°C to +85°C).
Pricing and Availability
The IDT family of UMPC timing devices (the 9UM9000 series and the 9UM700 series) is currently shipping in production and is available in 32 pins to 56 pins with QFN and SSOP packages. The commercial-grade IDT UMPC solutions range in price from $1.25 to $1.95 for 10,000 units. For additional information on the devices, visit www.idt.com/go/UMPC.
About IDT Timing Solutions
IDT is a leading provider of timing solutions for communication, storage, industrial and digital consumer applications. The IDT portfolio of silicon timing devices offers differentiated solution elements, such as programmable platform, precision technology, advanced I/O and stratum-compliant synchronization. Specific families include devices for clock generation, programmable skew, zero delay and non-Phase Locked Loop (PLL)-based clock fanout. For additional information on IDT timing solutions, visit www.idt.com/go/timing.
With the goal of continuously improving the digital media experience, IDT integrates its fundamental semiconductor heritage with essential innovation, developing and delivering low-power, mixed signal solutions that solve customer problems. Headquartered in San Jose, Calif., IDT has design, manufacturing and sales facilities throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT is available at www.IDT.com.
###
IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.