The Collaboration Will Enable Accelerated Development of Third-Generation RapidIO Switches While Expanding the RapidIO Ecosystem

July 8, 2014

SAN JOSE, Calif., July 8, 2014 – Integrated Device Technology, Inc. (IDT®) (NASDAQ: IDTI) and eSilicon Corporation announced today a collaboration to expedite development of next-generation RapidIO® switches to meet the growing performance demands of new system architectures for wireless, embedded and computing infrastructures. The two companies will work together to initially research and develop RapidIO switches operating at 40 Gbps per port based on the RapidIO 10xN specification.

Switches developed under this program will enable manufacturers of next-generation wireless base stations, Cloud RAN (radio access network), mobile-edge computing and other evolving carrier networks to stay ahead of mushrooming data usage accompanying the burgeoning use of portable devices.

“From design to implementation and volume manufacturing, this collaborative R&D effort is being established to expedite to market a new generation of RapidIO products to address the needs of higher-capacity, higher-bandwidth base stations and other carrier platforms,” said Jack Harding, CEO of eSilicon. “eSilicon’s expertise in 28-nanometer implementation, including high-speed SerDes deployment and custom memory design, is an excellent complement to IDT’s expertise in RapidIO designs.”

The RapidIO 10xN switches will offer an optimal combination of low 100ns latency, 40 Gbps per port of bandwidth and scalability to greater than 4 billion nodes in a network.  The jointly developed devices will target the new generation of base station platforms such as LTE-Advanced (LTE-A), C-RAN, and 5G, but will also find use in emerging architectures such as base stations co-located with high-performance computing (HPC) platforms.

IDT’s production 20 Gbps per port switches are currently the de facto interconnect standard for the clustering of DSPs, microprocessors, and ASICs in existing 3G and 4G base stations deployed worldwide. Under the collaboration, the companies will build on the current production switch and bridge portfolio, with plans to make their first jointly developed products available in the second half of 2015.

“Advancements in interconnect are essential for the continued evolution of communications infrastructure,” said Gregory Waters, CEO of IDT. “Our existing RapidIO switches are designed into virtually every 4G base station in the world. But the next generation of base stations and C-RAN is on its way, demanding higher performance than ever before. Joining efforts with eSilicon enables us to accelerate RapidIO development, to the benefit of our customers and the communications industry as a whole.”

“This collaboration between IDT and eSilicon, which will move RapidIO technology to 40 Gbps per port and beyond going to 100 Gbps, is a significant step forward for the growing RapidIO ecosystem,” said Rick O’Connor, executive director of RapidIO.org. “There’s no doubt this collaboration will be welcomed by developers of performance-critical computing applications requiring increased bandwidth and capacity, and will accelerate the deployment of RapidIO 10xN technology by processor, DSP and FPGA partner companies in the RapidIO ecosystem.”

About IDT
Integrated Device Technology, Inc. develops system-level solutions that optimize its customers’ applications. IDT uses its market leadership in timing, serial switching and interfaces, and adds analog and system expertise to provide complete application-optimized, mixed-signal solutions for the communications, computing and consumer segments. Headquartered in San Jose, Calif., IDT has design, manufacturing, sales facilities and distribution partners throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT is accessible at www.IDT.com. Follow IDT on Facebook, LinkedIn, Twitter, and YouTube.

About eSilicon
eSilicon, a leading independent semiconductor design and manufacturing solutions provider, delivers custom ICs and custom IP to OEMs, independent device manufacturers (IDMs), fabless semiconductor companies (FSCs) and wafer foundries through a fast, flexible, lower-risk, automated path to volume production. eSilicon serves a wide variety of markets including communications, computing, consumer, industrial and medical. www.esilicon.com.

eSilicon — Enabling Your Silicon Success™

###

IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. eSilicon is a registered trademark, and the eSilicon logo and Enabling Your Silicon Success are trademarks, of eSilicon Corporation. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.

Share this news on