Intersil's New Power Factor Controller Provides Low Harmonic Distortion, Maximum Efficiency Over Wide Voltage Ranges

ISL6730A Featuring New Negative Capacitance Technology Ideal for AC/DC Adaptor and Power Supply Applications

10 Apr 2013

Stock Price
Investor Relations

MILPITAS, CA -- (Marketwired) -- 04/10/13 -- Intersil Corporation (NASDAQ: ISIL), a world leader in the design and manufacture of high-performance analog, mixed signal and power semiconductors, has introduced a new active power factor controller that delivers minimal harmonic distortion (THD) and high power factor (PF) correction.

 

The ISL6730A features a patent-pending breakthrough in negative capacitance technology which reduces EMI filter size, improves THD and PF and provides maximum efficiency over a wide input supply range and output power (input voltages from 85VAC to 270VAC and power range from 50W to 2kW). This technology also minimizes zero crossing distortion, compensates for input filter capacitance PF displacement error and reduces the magnetic component size by up to 66 percent. For example, in an 85W power supply, the EMI filter inductor can be reduced from 150uH to 56uH. The small external components result in a lower cost design with improved performance.

 

The device's excellent power factor correction capability is compatible with the requirements for a power factor higher than 0.9, as currently required by ENERGY STAR Program Requirements for Computers Version 5.0. The ISL6730A also achieves excellent light load efficiency using integrated skip-mode, and includes an internally clamped 12.5V gate driver delivering 1.5A peak current to the external power MOSFET.

 

Fully Protected, Reliable Systems

The ISL6730A enables a reliable system that is fully protected with features such as cycle-by-cycle over-current, power limiter, over-temperature, input brownout, output over-voltage and under-voltage protection.

 

Features and Specifications

  • Negative capacitance generator reduces component size requirements
  • Excellent power factor and total harmonic distortion over a wide supply and output power range
  • Excellent light load efficiency
  • Internally clamped 12.5V gate driver delivers 1.5A peak current to the external power MOSFET

 

Pricing and Availability

The ISL6730A is available now in compact 10-lead MSOP package, with prices starting at $0.95 each in 1,000-unit quantities.

 

For more information please visit: 
http://www.intersil.com/products/ISL6730A

 

Intersil and the Intersil logo are trademarks or registered trademarks of Intersil Corporation. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.

 


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.