图像
Tetsuji Tsuda
Tetsuji Tsuda
Principal Engineer
已发布: 2020年9月16日

Want to develop motor control software safely?

Want to develop motor control software based on operability confirmed software?

Want to reflect the result into motor control software after motor parameter measurement?

Want to figure out the reason the motor stopped rotating unintentionally?

I am writing this article for the persons who want the above requests.

Nice to meet you, I am Tetsuji Tsuda from Renesas.

Renesas provides an xEV Inverter Reference Solution.

xEV Inverter Reference Solution

The xEV Inverter Reference Solution consists of hardware and software to control xEV motors.

I’m in Software development.

The xEV Inverter Reference Solution software provides the following content for the above requests.

Want to develop motor control software safely?

  • Measure current, voltage, temperature, and rotation speed and if these values are over defined values, the motor will stop rotating
  • Monitor measured components and if an abnormality is found, the motor will stop rotating

Want to develop motor control software based on the operability of confirmed software?

  • Provides not only microcontroller unit control software but also motor control software
图像
xev-inverter-reference-solution-diagram

 

Want to reflect the result into motor control software after motor parameter measurement?

  • Provides documents describing the motor’s resistance, inductance, interlinkage magnetic flux, and position gap measurement method, and software reflection method. Furthermore, provides the required software to measure the position gap

Want to figure out the reason the motor stopped rotating unintentionally?

  • Store the reason to stop rotating the motor into Flash memory

The xEV Inverter Reference Solution software contributes to a customer’s development time reduction.

If you are interested, please contact our sales team