StarBridge RapidExpress Bridge Card and Switch Box Products Featuring IDT Solutions Enable PC Aggregation over RapidIO for High Performance, Multiprocessor Applications
2012年3月14日

 

SAN JOSE, Calif., October 3, 2011 – Integrated Device Technology, Inc. (IDT®; NASDAQ: IDTI), the Analog and Digital Company™ delivering essential mixed-signal semiconductor solutions, today announced that StarBridge, Inc. has selected IDT’s PCI Express Gen 2 to RapidIO Gen 2 bridge and RapidIO Gen 2 switch for its RapidExpress products that enable easy aggregation of high performance compute and I/O nodes via a high speed RapidIO network at 20 Gbaud per link. The IDT-enabled RapidExpress solutions are ideal for prototype and production systems in industrial, imaging and server applications.

          The IDT Tsi721 PCI Express (PCIe) to Serial RapidIO bridge is at the heart of the StarBridge RapidExpress bridge card solution, enabling the translation of the PCIe protocol to RapidIO and vice versa at up to 20 Gbaud. The PCIe protocol allows for Intel, AMD and other PCIe-enabled processors to be used in a large peer-to-peer multi-processing environment, while the Serial RapidIO protocol provides a scalable, high-throughput, low-latency, fault tolerant interconnect for straightforward architecting of peer-to-peer processing clusters. The IDT solution offers superior throughput, latency and overall system-level power as compared to solutions for other interconnect protocols such as 10GigE and InfiniBand®.

          In addition, the RapidExpress bridge card is complemented by the StarBridge RapidIO switch box, which utilizes the IDT CPS 1432 to provide eight x4 Serial RapidIO Gen 2 ports via Quad Small Form-factor Pluggable (QSFP) connectors with support for copper or optical transceivers.  Eight processor node systems can be connected with one RapidExpress switch and eight bridges. Larger systems can be created by simply cascading multiple switch boxes with up to 64K endpoints.

          “The StarBridge RapidIOExpress bridge and switch products using the IDT Tsi721 and IDT CPS1432 are ideal for customers to quickly develop large multi-processor systems with Intel or other PCIe enabled CPUs using a RapidIO network,” said Fred Zust, vice president of the Communications Division at IDT. “The combination of these StarBridge products, enabled by IDT silicon, allow customers to create scalable, low latency, reliable systems that are not possible using other interconnect technologies.”

          IDT is the leader of RapidIO bridging and switching ICs, consistently releasing the world’s most advanced solutions. For more information about IDT’s RapidIO bridge and switch portfolio, visit www.idt.com/go/S-RIO. The RapidExpress bridge card and switch box are available worldwide directly from StarBridge. Information on these products can be found at www.starbridge.co.jp or via email at contact@starbridge.co.jp.


About IDT
          Integrated Device Technology, Inc., the Analog and Digital Company™, develops system-level solutions that optimize its customers’ applications. IDT uses its market leadership in timing, serial switching and interfaces, and adds analog and system expertise to provide complete application-optimized, mixed-signal solutions for the communications, computing and consumer segments. Headquartered in San Jose, Calif., IDT has design, manufacturing and sales facilities throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT is accessible at www.IDT.com. Follow IDT on FacebookLinkedInTwitter, and YouTube.

###

IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.

分享此文章

分享此文章