Low Voltage Motor Control with Enhanced Operation

Low Voltage Motor Control with Enhanced Operation

Reducing power consumption, physical size, and design costs are key challenges in the consumer appliance industry. Renesas offers a wide range of MCUs tailored for motor drive applications.

RZ/V Defect Detection in the Industrial Field

産業分野におけるRZ/V MPU を使用した欠陥検出

本稿では、プリント基板の欠陥検出を例に、YOLOv3-tiny欠陥検出AIアルゴリズムの構成、展開プロセス、ルネサスRZ MPUにおける推論性能について紹介する。

RX26T new lineup expansion : Suitable for Motor Control Applications

モータ制御アプリケーションに最適なRX26Tの製品ラインアップを拡充

RX26Tグループの新たな製品ラインアップとして、RX26T(RAM48KB)製品をリリースしました。モータ/インバータ制御向けに、より高性能/高機能なマイコンをお探しの方、ぜひご覧ください。

Renesas Powers a New Space Race

ルネサスが新たな宇宙開発競争を加速させる

月面への着陸が話題となっている宇宙ですが、最近は「ニュースペース」と呼ばれる民間による宇宙産業も活況を呈しています。何が起こっているのか、ルネサスの宇宙ビジネスへの取り組みと共に解説します。

Experience Digital Signal Processing  with RX MCU on the Cloud!

DSPを体感しよう!RXマイコンを使ったDSPシステムにオンラインでアクセス!

オンラインでRXマイコンの評価ボードに接続し、DSPを体感できるLab on the CloudのRXファミリDSPソリューションを紹介します。

<style type="text/css">@media (min-width: 996px) { .col-lg-7.first_blog_p { padding-left: 50px; }} @media (max-width: 995px) { .col-lg-7.first_blog_p { padding-top: 50px; }} </style> <div class="row"> <div class="col-lg-5" style="padding: 20px 20px 0px 20px;border: 1px solid #e1e0e0; border-radius: 4px;"> <h4>Radar Transceivers: Key Components for ADAS &amp; Autonomous Driving</h4>  <ul> 	<li><a data-entity-substitution="canonical" data-entity-type="node" data-entity-uuid="d18059ba-52f0-4c58-9978-db1070c9bd

How to connect the antennas?

At mmWaves the interfaces between the radar MMIC and the antennas need to be carefully designed to avoid any degradation on the system performance. This issue of the blog will highlight some aspects that need to be considered in the design of the transitions for different antenna configurations.

Configuration Issues with the RA6 Ethernet Controller

Configuration Issues with the RA6 Ethernet Controller

Are you having issues with the Ethernet controller on the RA6 MCU family? This blog suggests that you should check the configuration of the Arm® TrustZone® boundaries and explains why.

Let's Make a Game Using a Microcontroller Blog - Part 2

マイコンを使ってゲームを作ろう!②

今回は、落ち物パズルの作成に挑戦します!ハードウェアの設計で使用した部材と回路図を紹介しています。ソースコードも公開しておりますので、是非作成してみてください。

Renesas RZ/G2M Awarded Arm SystemReady IR 1.1 Certification

Renesas RZ/G2M Awarded Arm SystemReady IR 1.1 Certification

The Renesas RZ/G2M platform is the first RZ/MPU platform to be officially certified by Arm as compliant with SystemReady IR 1.1, a set of interoperability specifications targeting edge and IoT devices.

Single MCU Solution for Safety-Related Applications Using TrustZone Blog

Single MCU Solution for Safety-Related Applications Using TrustZone

Learn how RA 32-bit MCUs enable implementing a Class C application on a single microcontroller.