MicroClock Devices Help Manufacturers Maximize Battery Life and Decrease Size of Smart Wearables, Sensor Modules and Other Small, Battery-Powered Devices

2019年7月30日

SAN JOSE, Calif., July 30, 2019 – Integrated Device Technology, Inc. (IDT), a wholly owned subsidiary of Renesas Electronics Corporation (TSE: 6723), today announced the availability of its new MicroClock™ family of clock generators, which are optimized for small, battery-powered devices, such as smart watches, hearables, fitness monitors, portable medical equipment and devices connected to the Internet of Things (IoT). The MicroClock devices are ideal for these products by combining a small form factor, low power consumption and programmability.

The extremely small size of MicroClock ICs – as small as 2 mm x 2 mm – in combination with the ability to output up to three unique frequencies can reduce the board space needed for timing devices by up to 80 percent. This is a key advantage for small, battery-powered devices, enabling product designers to increase battery size or shrink the overall size of the product. Additionally, the MicroClock family supports up to three unique frequency outputs which reduces board space requirements by eliminating the need for multiple, discrete crystal oscillators, as well as providing a more reliable clock source.

Complementing its size advantages is the ultra-low power consumption of the MicroClock series, which is less than 1 μA thanks to its low-power 32.768 kHz clock that supports system Real Time Clock (RTC) needs. This low power consumption maximizes battery life, a key advantage for smart wearables and other consumer devices as they can operate longer between charges. Low power is also important for IoT-connected sensors used in smart city, industrial and other applications that operate where electrical power is unavailable.

The exceptional programmability of MicroClock devices means it can easily be configured to meet the specific requirements of each application, making it a highly flexible solution that can accelerate time-to-market. Key examples include support for up to three unique frequency outputs and programmable VCO and PLL source selection, which enables users to optimize power consumption based on the specific requirements of their applications.

“IDT’s MicroClock family of clock generators enables manufacturers to get smart wearables, fitness monitors and other small, battery-powered devices to market faster thanks to a combination of programmability, small size and low power,” said Bobby Matinpour, vice president and general manager of IDT’s Timing Products Division. “With MicroClock devices, manufacturers can simultaneously meet their key goals of maximizing battery life while decreasing the overall size of their devices.”

IDT’s MicroClock line of programmable clock generators is currently comprised of four devices – the new 5X1503 and 5L1503 along with 5X2503 and 5L2503 – which are all available today. Visit idt.com/microclock to learn more and request samples.

About IDT

Integrated Device Technology, Inc., a wholly owned subsidiary of Renesas Electronics Corporation (TSE: 6723), develops system-level solutions that optimize its customers’ applications. IDT’s market-leading products in RF, high performance timing, memory interface, real-time interconnect, optical interconnect, wireless power and smart sensors are among the company’s broad array of complete mixed-signal solutions for the communications, computing, consumer, automotive and industrial segments. Headquartered in San Jose, Calif., IDT has design, manufacturing, sales facilities and distribution partners throughout the world. Additional information about IDT can be found at www.IDT.com. Follow IDT on Facebook, LinkedIn, Twitter, and YouTube.

###

© 2019, Integrated Device Technology, Inc. IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc., and its worldwide subsidiaries. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.

この記事をシェアする