NOTICE - This software / tool has been discontinued. Please contact technical support with any questions.
The PG-FP5 installed in a system is a tool for erasing, programming, and verifying programs on Renesas MCUs with on-chip flash memory.
The PG-FP5 has been discontinued. The acceptance of final orders was in May 2018. If adopting new products, please consider the successor, the PG-FP6.
[PG-FP6] Higher productivity and security than its predecessor, PG-FP5 >>
Note: the PG-FP6 does not support V850 and 78K with dual power supply flash memory, which assume mass production with mask ROM. Use programmers produced by partners for programming of the V850 and 78K with dual power supply flash memory. Refer to Function and performance comparisons between PG-FP6 and PG-FP5 >>
Latest Ver.: V2.17
Released: Apr 22, 2019
Latest Ver.: V2.17
Released: Apr 22, 2019
Latest Ver.: V4
Released: Jul 15, 2011
Latest file released: Apr 20, 2022
Details of upgrade(See Tool News)
How to find the version number
For details of support for individual device part numbers, see List of MCUs supported by PG-FP5 (PDF | English, 日本語) (incl. information on components and parameter files).
Note: Except for Europe, the power supply adapter, QB-COMMON-PW-xx, is not bundled in the product package of PG-FP5. Please purchase it separately.
To check the version number, follow these steps: