PM2.5 Monitor with Portable Battery

Renesas demonstrates the PM2.5 Monitor with Portable Battery quick solution featuring the RL78/L12 microcontroller. This is a portable device that can measure and detect the concentration of PM2.5, an air pollutant in real-time. This monitoring solution has two functions: PM2.5 concentration testing functions and portable power.