iSim:PE v7.0 Lets Users Quickly Sort and Select, Add Jumpers for Easy Circuit Configuration

August 27, 2013

MILPITAS, CA -- (Marketwired) -- 08/27/13 -- Intersil Corporation (NASDAQ: ISIL), a leading provider of innovative power management and precision analog solutions, today introduced the latest version of its popular iSim™ Personal Edition (iSim: PE) circuit simulation design tool, adding time saving features and further simplifying part selection for power and analog IC designers.

 

Intersil's iSim:PE v7.0 speeds the design cycle and reduces risk early in any project, identifying parts that can be used in current as well as next-generation designs. The easy to use tool quickly and reliably selects devices to support increasing power densities, wide input-voltage and temperature ranges, maximum efficiency, fast transient response and other vital specifications. Simulated designs are displayed in an online schematic and can be verified immediately. After verification, iSim generates a Bill of Materials and a comprehensive design report.

 

New to this release is a tool to quickly search, review and select MOSFETS or diodes based on design requirements, letting users easily filter and sort from all available devices. A new feature allows designers to add jumpers, enabling easily switching between different circuit configurations. Jumpers are electrically modeled as opens or shorts and are compatible with SIMPLIS® for power management parts and SIMetrix™ for analog ICs.

 

The new iSim:PE v7.0 is available free-of-charge from Intersil at http://www.intersil.com/iSim. To see the iSim tool in action, watch this short video http://www.intersil.com/en/tools/iSim.html

 

Intersil, iSIM and the Intersil logo are trademarks or registered trademarks of Intersil Corporation. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

Share this news on