Skip to content

renesas/ra-fsp-examples

Folders and files

NameName
Last commit message
Last commit date

Latest commit

 
 
 
 
 
 
 
 
 

Repository files navigation

Overview

Examples for Renesas RA MCU family include Example Projects and Application Projects

Example Projects

Example projects demonstrate the basic usage of FSP in user applications

Instructions For Running Example Projects

  1. Refer to the FSP version requirements table per IDE to correctly download the needed FSP release.
  2. Refer to the 'Example Project Usage Guide' document in the 'example_projects' folder for steps and information on importing and running the projects.
  3. Example Projects source code for modules supported on each kit is in \example_projects\kit\module folder.
  4. Projects for each of the kits can be downloaded from 'Assets' section of 'releases'. e2studio folder includes pre-compiled binary and source code.
  5. 'readme.txt' file in each of the module folders provides a brief description of the example project and hardware requirements for running the projects.

Application Projects

Application Projects illustrate solutions in various core technologies

Instructions For Running Application Projects

  1. Refer to the 'Application Note' in the project folder for steps on importing and running the projects.
  2. Application Projects source code is in \application_projects\technology folder.
  3. Projects can be downloaded from 'Assets' section of 'releases'.

Third Party App Notes

Keil MDK App Note: http://www.keil.com/appnotes/docs/apnt_330.asp

References

  1. FSP Webpage: www.renesas.com/ra/fsp
  2. FSP GitHub: https://github.com/renesas/fsp
  3. FSP Releases: https://github.com/renesas/fsp/releases
  4. FSP Documentation: https://renesas.github.io/fsp
  5. RA Product Information: www.renesas.com/ra
  6. RA/FSP Knowledge Base: https://en-support.renesas.com/knowledgeBase/category/31087
  7. Support: www.renesas.com/support