1. Home

Renesas Synergy™ Solutions

Renesas Synergy™ Solutions kits go beyond typical embedded product development kits to offer actual products examples, and to offer bundled technologies, giving you a head start on your own hardware designs.

 

Renesas Synergy™ Solutions come in two categories: Product Examples (PEs) kits and Application Examples (AEs) kits.

 

 

Product Example (PE)

Product Examples are solutions that offer a guide post into a "design instance" of a particular end-product. A PE closely represents how an actual end-product may be designed. As a time saver, portions of the Renesas Synergy™ PE designs can be reused in actual end-products. The PE designs can also be leveraged by using the design journey documentation which describes the decision process made by the original PE designers. This enables developers the ability to modify the PE design to meet their particular needs. PE design journeys document the methodology of how and why design choices were made and the reasoning behind the selection of components and methodologies.

 

PEs offer complete and optimized hardware design with full documentation, a bill of materials (BOM), and Gerber files for PC board layout.

 

Ordering Kits

Americas Europe Japan
Arrow Renesas Shop Chip One Stop

Avnet

  Marutsu
Digi-Key    
Future    
Karimex (Brazil only)    

 

 

PE-HMI1

Human Machine Interface

 

  • Based on Renesas Synergy™ S7 Series MCUs
  • 7" WVGA TFTLCD with capacitive touch overlay
  • High speed wired and wireless connectivity
  • Ethernet, USB-HS Host and Device, Wi-Fi, Bluetooth and BLE, CAN, SDHI, camera, RS232/RS485

 

PE-DAQ1*

Data Acquisition

 

  • Based on Renesas Synergy™ S3 Series MCUs
  • Industrial environmental monitor
  • Sensor fusion, low power
  • IEEE-802.15.4 6LoWPAN mesh network
  • Motion, humidity, temperature, pressure, light sensors

 

PE-SNS1*

Smart Network Sensor

 

  • Based on Renesas Synergy™ S1 Series MCUs
  • Motion detector / occupancy sensor
  • BLE
  • AAA battery powered

 

* Currently Planned

 

Renesas Synergy™ Solutions: Application Example

Application Examples are kits which include multiple components creating a showcase of the use of multiple technologies surrounding and including the Renesas Synergy™ Platform. Combining Development kits, Product Examples, Renesas Synergy™ VSA and QSA software add-ons, and hardware plug-ins and components from other vendors, these all-inclusive kits are all about solutions. From wired or wireless networking, connectivity protocols, smart sensors, security and encryption, functional safety to capacitive touch or motor control, AEs provide a massive head start on new designs. All AEs are fully documented with an application note and include SSP-based e2 studio software projects.

 

AE-CAP1*

Capacitive Touch

 

Technologies Highlighted:

 

  • Renesas third-generation touch technology
  • Auto-tuning

 

 

* Currently Planned

Confirm below disclaimers

Input Renesas account name and password

Usando os filtros abaixo você pode filtrar os programas exemplo e as notas de aplicação que são mostradas.

Confirm below disclaimers

Input Renesas account name and password

Disclaimer:

The information contained herein has been provided by a member of Renesas Partners. This information is provided on the Renesas website provided for convenience and informational purposes only. Renesas is not responsible for the contents of this page or any changes or updates to the information posted on this page. Certain links provided herein permit you to leave this site and enter non-Renesas sites. These linked sites are not under control of Renesas. Renesas is not responsible for the contents of any linked site or any changes or updates to such sites. These links are provided for convenience and informational purposes only. The inclusion of any link does not imply endorsement by Renesas of any linked site.

Renesas's Publication of information regarding third-party products or services does not constitute an endorsement regarding the suitability of such products or services or a warranty, representation or endorsement of such products or services either alone or in combination with any of Renesas's product or service.

Contact