概览

简介

Topics
[Upgrade to Revision] C Compiler Package for RL78 Family [CC-RL] V1.13.00 (PDF | English, 日本語)
    V1.13.00 has expanded functionalities including an addition of the library generator.

In development of embedded systems, C Compilers for RL78 Family offers the powerful optimizations for enhancing execution speed and code efficiency, and the utilities to increase productivity. Products differ depending on each integrated development environment.

 

特性

  • https://www.renesas.com/us/en/document/rln/rl78-compiler-cc-rl-v11201-release-noteANSI-compliant
    • Support C89, C99 of ANSI
      Note: The variable length array type, complex type, and some standard library functions of the C99 standard are not supported.
  • Superior optimization
    • The compiler applies our latest optimization techniques to generate code that has excellent performance in execution (up to a three-fold (Measured for programs held by Renesas) improvement in execution performance over code compiled by the CA78K0R compiler, our previous product)
    • The compiler applies our latest optimization techniques to the generation of compact code (up to a 10-percent (Measured for programs held by Renesas) improvement over the CA78K0R).
    • Easy optimization settings and many optimization features
    • Linker-level optimization is now included in addition to optimization at the compiler level.
  • Cooperated with RL78 MCU architecture
    • Interrupt processing routines can be written in the C language (up to a six-fold (Measured for programs held by Renesas) improvement in interrupt response performance over code compiled by the CA78K0R compiler)
    • Provides intrinsic functions
  • An MISRA C rule checker supports the description of high-quality program [Professional edition only]
    • Supports automatic checking of C source code based on the MISRA-C: 2004/2012 rules as compiler options
    • About MISRA C, refer to here. [Learn More]
  • Assistance in Porting Files to the CC-RL from the CA78K0R. [Learn More]
  • Learn More

发布信息

目标设备

下载

文档

Order

When purchasing a compiler package, contact your nearest distributor.
Alternatively, Web sites for online sales are accessible by clicking on a [Buy/Quote] button in the table below.

  • We offer various licenses to suit a range of needs. Refer to Compiler Licenses for details.
  • The license keys of the compiler included in the packages for each of the products are usable with either CS+ or the e² studio.
    In the Americas and Europe, use the e² studio instead of the CS+.
  • The C Compiler Package no longer includes the installation medium (CD/DVD).
    Please obtain the installer from each product page.
  • 1.01.00 or later versions of CC-RL support both floating licenses and annual licenses.

 

Licenses for Newly Purchasing the Latest CC-RL

Give the part number from the list below to the distributor. Web sites for online sales are also accessible by clicking on a [Buy/Quote] button in the table below.

Important
Each of the compiler packages listed below comes with a license which allows you to use the latest version of CC-RL.
RL78 Family C Compiler PackageOnline Sales
PeriodForm of usageEditionPart NumberMouserAvnetchip1stop
annualNode-LockedstandardLow price
RTCRL7800CB01WNR
Buy/QuoteBuy/QuoteBuy/Quote
professionalRTCRL7800CA01WNRBuy/QuoteBuy/QuoteBuy/Quote
FloatingstandardRTCRL7800CB01WNRN1Buy/QuoteBuy/QuoteBuy/Quote
professionalRTCRL7800CA01WNRN1Buy/QuoteBuy/QuoteBuy/Quote
permanentNode-LockedstandardRTCRL7800CS01WNRBuy/QuoteBuy/QuoteBuy/Quote
professionalPopular item
RTCRL7800CL01WNR
Buy/QuoteBuy/QuoteBuy/Quote
FloatingstandardRTCRL7800CS01WNRN1Buy/QuoteBuy/QuoteBuy/Quote
professionalRTCRL7800CL01WNRN1Buy/QuoteBuy/QuoteBuy/Quote

For multiple licenses, the end of the part number depends on the number of licenses.

  • For Node-Locked licenses, L5, LA, or LT is added at the end of the part number depending on the number of licenses (5, 10, or 20).
    (For example, when the number of licenses is 5, the part number is RTCRL7800CL01WNRL5
  • For Floating licenses, the last numeric character “1” at the end of the part number is replaced by 5, A, or T depending on the number of licenses (5, 10, or 20).
    (For example, when the number of licenses is 5, the part number is RTCRL7800CL01WNRN5

 

License for Upgrading from the CC-RL Standard Edition to the Professional Edition

Give the part number from the list below to the distributor. Web sites for online sales are also accessible by clicking on a [Buy/Quote] button in the table below.

C Compiler Package for RL78 Family V1 Upgrade (Edition)Online Sales
PeriodForm of usagePart NumberMouserAvnetchip1stop
permanentNode-LockedRTCRL7800CU01WNRBuy/QuoteBuy/QuoteBuy/Quote

Note:

  1. Node-Locked license for CC-RL standard version (permanent) is required.
  2. This form of upgrade (of the edition) is only for node-locked licenses; it will not apply to floating licenses and annual licenses.

For multiple licenses, the end of the Part Number changes depending on the number of licenses.

  • For Node-Locked licenses, L5, LA, or LT is added at the end of the part number depending on the number of licenses (5, 10, or 20).
    (For example, when the number of licenses is 5, the part number is RTCRL7800CU01WNRL5

 

License Requirements

Regardless of whether you have a license or not, all versions of CC-RL can be used for commercial purposes such as development and production. If you will be using the CC-RL beyond the restrictions on the linkage size or optimization or would prefer to use the professional edition, consider purchasing a license for CC-RL.

For more information on the trial period and types of license, see Compiler Licenses.

Purpose (Field) of UsageFeature  License
Evaluation of the features and performance of compiler products
Commercial usage
Standard edition (basic features)Applicable restrictions Note1V1.11.00 or earlier versions: Linkage size
V1.12.00 or later versions: Optimization
No restriction lens
Professional edition (advanced features)  lens
Technical support (contact)   lens

lens Required | — Not required

Note:

  1. Applicable restrictions
    • V1.11.00 and earlier versions: The linkage size is no more than 64 KB.
    • V1.12.00 and later versions: The only available levels of optimization are -Onothing (debug precedence) or -Olite (partial optimization).

 

Related Services

Compiler Qualification (Service to Support Functional Safety)

For customers who are using a compiler for Renesas devices, we offer a support service for the qualification of confidence that development tools meet the requirements of ISO 26262, Road Vehicles Functional Safety. This service incurs a charge.
Compiler Qualification

Compiler Maintenance Service (Agreement for Maintenance Service for a Specified Compiler Version)

Renesas offers a maintenance service for a specific compiler version for customers who are using the compiler over the long term. This service incurs a charge.
Compiler Maintenance Service

Assistance with Compiler Migration

The IDEs from Renesas (such as the e² studio and CS+) allow for the porting of projects between IDEs to facilitate the reuse of existing resources. Refer to the guidance page of migration when changing your compiler after changing your development environment. The guidance page describes precautions that must be taken when changing compilers, such as differences in options and in extended language specifications.
Migrating between Integrated Development Environments

图像