工业领域的 RZ/V 缺陷检测
本文以 PCB 缺陷检测为例,介绍 YOLOv3-tiny 缺陷检测人工智能算法的结构、部署过程以及在 Renesas RZ MPU 中的推理性能。
本文以 PCB 缺陷检测为例,介绍 YOLOv3-tiny 缺陷检测人工智能算法的结构、部署过程以及在 Renesas RZ MPU 中的推理性能。
作为RX26T产品群阵容的新成员,我们推出了RX26T(RAM48KB)产品。若您正在寻找针对电机/逆变器控制的更高性能/更多功能的单片机,那么绝对不容错过。
Blog discussing Renesas’ High Rel business
本期将为大家介绍的是Lab on the Cloud中的RX产品家族DSP解决方案,通过该方案用户可以在线连接RX单片机的评估板并体验DSP。
At mmWaves the interfaces between the radar MMIC and the antennas need to be carefully designed to avoid any degradation on the system performance. This issue of the blog will highlight some aspects that need to be considered in the design of the transitions for different antenna configurations.
Are you having issues with the Ethernet controller on the RA6 MCU family? This blog suggests that you should check the configuration of the Arm® TrustZone® boundaries and explains why.
This blog introduces the components and circuit diagram used in the hardware design to build a falling block puzzle game with an RL78 microcontroller. The source code is also available.
The Renesas RZ/G2M platform is the first RZ/MPU platform to be officially certified by Arm as compliant with SystemReady IR 1.1, a set of interoperability specifications targeting edge and IoT devices.
Learn how RA 32-bit MCUs enable implementing a Class C application on a single microcontroller.
This blog looks at how we can automate a series of SPI transfers using the command sequencer implemented on many RA 32-bit MCU devices.