NFC Revolutionizing IoT Applications: A Seamless Future
Embrace the future of connectivity and enhance your application with Renesas’ PTX105R NFC controller for Internet of Things applications, the most suitable NFC reader on the market.
Embrace the future of connectivity and enhance your application with Renesas’ PTX105R NFC controller for Internet of Things applications, the most suitable NFC reader on the market.
在这篇博客中,我将介绍如何使用Chat-GPT和与Arduino兼容的RL78板进行AI编程,以及其实际应用示例。
Blog discussing Renesas’ memory interface solutions
Introduction to Renesas solutions for smart agriculture
With the ubiquity of wireless connectivity options on IoT devices, connection to the cloud has become more flexible than ever. Traditionally, Wi-Fi has been the most popular choice in the IoT world although this has changed in recent years with the huge strides made in cellular networks. However, there is no right answer for which option would be the best or the more efficient between the two.
The type of network connection to use depends on several factors that affect solution development.
The AIoT has been enabled by higher MCU compute capability and thin neural network models that are more suited for edge and end point devices than traditional CPUs and MPUs.
We’ll create a digital angle meter using the RL78/G15 Fast Prototyping Board. The data from the gyro sensor will be converted into angles and displayed on the LCD.
By using the standalone version of QE for Capacitive Touch, you can develop capacitive touch applications even with IAR's EWRX IDE.
Introducing the RZBoard V2L, a small single-board computer that enables easy Vision-AI trial with the RZ/V2L MPU.
在这篇博客中,我们将讨论电快速瞬变 (EFT) 是如何引起的,如何测量收发器 EFT 性能,以及 RS-485 收发器的 EFT 测量结果。