图像
Tetiana Fedorchuk
Tetiana Fedorchuk
Lead Generation Coordinator
已发布: 2021年5月21日

Renesas launches Wi-Fi Provisioning App, which is now available for use on Google and Apple Stores. The Wi-Fi Provisioning App is a mobile application from Renesas that works with development kits supported by Renesas' DA16200 and DA16600 Wi-Fi SoCs. Using the app, you can configure the Wi-Fi network connection of the DA16200 and DA16600, and establish a connection to the Wi-Fi network.

The license-free example source code is available for both iOS and Android as an example implementation of Wi-Fi provisioning for DA16200. To download the source code, you need to register on the website.

Simply download the Renesas Wi-Fi Provisioning App from Google Play or Apple Stores. Check the User Manual for the mobile app to connect your DA16200 to the Wi-Fi network.