IDT Presents Wide Dynamic Range Power Meter ICs and Demonstrates New Power, Touch, Clocking and Video Products

2011年2月10日

 

SAN JOSE, Calif., February 10, 2011 – Integrated Device Technology, Inc. (IDT®; NASDAQ: IDTI), the Analog and Digital Company™ delivering essential mixed-signal semiconductor solutions, today announced that it will be exhibiting its latest products at the IIC-China Conference and Exhibition in Shenzhen, China on February 24-26, 2011. Product demonstrations will be on display in booth 2F15 on the main showroom floor. IDT will also be speaking at IIC China, showcasing the industry’s widest dynamic range power metering products.

 

          The IIC China 2011 Spring conference comes at a great time for IDT to showcase several new and exciting products poised to gain strong traction in China this year. Such products to be exhibited include the industry’s first true single-layer projected capacitive touch screen technology with complementary controller IC, the highly flexible VersaClock® III programmable output clocking family, the powerful HQV™ Vida advanced video processing device, and industry’s widest range power metering ICs.

          In addition, IDT will deliver a presentation introducing the IDT90E2x family of wide dynamic range energy metering products. The presentation will cover the design of a 1 A to 100 A wide-span single-phase energy meter and the numerous benefits of using the IDT90E2x device. Recent energy meter designs using the IDT90E2x devices at Gude GmbH and Sanxing reinforce the value of IDT’s superior solutions.

          “China is a very important region for IDT. Our talented analog and digital engineers at our China design facility and other IDT design facilities throughout the world are focused on creative designs to meet the needs of this growing market and beyond,” said Sean Fan, vice president and general manager of IDT China. “Our growing portfolio of innovative mixed signal products emphasizes IDT’s commitment to maintaining market leadership. Early design wins and positive feedback for our new products are evidence that our focus is proving successful.”

          IDT’s power metering presentation at IIC China will be held from 2:00pm to 2:50pm CST on February 24, 2011 in conference room 1, hall 2, in the Shenzhen Convention & Exhibition Center.

About IDT
Integrated Device Technology, Inc., the Analog and Digital Company™, combines analog and digital technology to develop system-level innovations that optimize customers’ applications and enrich the end-user experience. IDT uses its market leadership in timing, serial switching and interfaces, and adds  analog and system expertise to provide complete application-optimized, mixed-signal solutions for the communications, computing and consumer segments. Headquartered in San Jose, Calif., IDT has design, manufacturing and sales facilities throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT is accessible at www.IDT.com. Follow IDT on Facebook, LinkedIn, Twitter, and YouTube.

###
IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.

 

分享此文章

分享此文章