IDT to Showcase Latest Innovations in Wireless Power and Wireless Infrastructure at Two Major Customer Events

2013年2月12日

SAN JOSE, Calif., February 12, 2012 – Integrated Device Technology, Inc. (IDT®) (NASDAQ: IDTI), the Analog and Digital Company™ delivering essential mixed-signal semiconductor solutions, today announced that it will be exhibiting innovative products from its industry-leading portfolio at Mobile World Congress (MWC) and IIC China. MWC will be held February 25-28 in Barcelona, Spain and IIC China will be held February 28 to March 2 in Shenzhen, China.

          IDT will demonstrate its portfolio of mixed-signal solutions for a variety of applications, with emphasis on solutions for wireless power and wireless infrastructure markets. IDT’s award-winning wireless power showcase includes magnetic inductance-based transmitter and receiver solutions that comply with the Wireless Power Consortium (WPC) Qi standard, ensuring interoperability with other devices that meet the Qi standard. The high-level integration of IDT’s solutions enable system designers to significantly reduce board area, cost, and component count to deliver superior wireless charging products in convenient and attractive form factors. IDT is also a member of the Power Matters Alliance (PMA), which currently has the largest installed base of magnetic inductance-based charging pads and sleeves, and growing partnerships with industry-leading retailers.

          Furthermore, IDT has partnered with both Intel and Qualcomm to develop wireless charging solutions for magnetic resonance-based charging technology, and is a member of the Alliance for Wireless Power (A4WP), a global organization for wireless power transfer technology focused on magnetic resonance. Next-generation magnetic resonance-based solutions will be on display at the show. For more information about IDT’s wireless power solutions, visit www.wirelesspowerbyidt.com.

          Innovative IDT offerings for wireless infrastructure applications will also be on exhibit, emphasizing the breadth of products that IDT provides for the entire signal chain of wireless infrastructure systems. These products include RF, high-speed data converters, RapidIO®, data compression, and timing solutions that provide a comprehensive system-solution. Recently announced 16-bit dual digital-to-analog converters with an industry-first JESD204B interface will be on display, along with innovative products from IDT’s expanding RF portfolio, including its Zero-Distortion™ RF mixers, FlatNoise™ variable gain amplifiers (VGAs), and Glitch-Free™ digital step attenuators (DSAs).

          In addition, demonstrations and examples of IDT’s leading timing portfolio will be at the conferences. Featured products will include members of the industry-leading silicon timing portfolio as well as IDT’s frequency control products, including CrystalFree™ MEMS oscillators and products from Fox Electronics, an IDT subsidiary.

          At MWC, the IDT booth will be located in hall 7, stand 7H41. At IIC China, the IDT booth will be located in hall 2, stand 2F26.

About IDT

          Integrated Device Technology, Inc., the Analog and Digital Company™, develops system-level solutions that optimize its customers’ applications. IDT uses its market leadership in timing, serial switching and interfaces, and adds analog and system expertise to provide complete application-optimized, mixed-signal solutions for the communications, computing and consumer segments. Headquartered in San Jose, Calif., IDT has design, manufacturing and sales facilities throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT is accessible at www.IDT.com. Follow IDT on Facebook, LinkedIn, Twitter, and YouTube.

###

IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.

分享此文章

分享此文章