The real-time OS aware debugging presented herein supports task-level debugging of real-time OS applications in the Integrated Development Environment High-performance Embedded Workshop. This function comes standard with High-performance Embedded Workshop. There is no need to rebuild the real-time OS, nor will overhead be incurred. (Debug patches, etc. are not necessary.)
When using Renesas real-time OSs, you can make use of extended debugger options that permit more detailed object status references (real-time OS debugger [Debugging Extension] task window, etc. and MR window of the PC7501 emulator, etc.). These windows include the items normally displayed in the OS object window. (The relationship between these windows and the OS object window is similar to the relationship between a watch window and local window.)
Refer to the help file of the E100 emulator for more information about the functionality.
Function | HI7200/MP, HI7750/4, HI7700/4, HI7000/4 |
RI600/4 | M3T-MR30/4, M3T-MR30 |
HI1000/4 | MR8C/4, Smalight OS |
---|---|---|---|---|---|
OS object | ✔ | ✔ | ✔ | ✔ | ✔ |
Task trace | ✔ | ✔ | ✔ | ✔ | ✔ |
Task analyze | ✔ | ✔ | ✔ | ✔ | ✔ |
OS trace | - | ✔ | ✔ | - | - |
OS analyze | - | ✔ | ✔ | - | - |
Task step | - | ✔ | ✔ | ✔ | ✔ |
Currently executed task display | - | ✔ | ✔ | ✔ | ✔ |
Execution history display | - | ✔ | ✔ | ✔ | ✔ |
Realtime profile | - | ✔ | ✔ | ✔ | ✔ |
Task specification | - | ✔ | ✔ | ✔ | ✔ |
Stack coverage | - | ✔ | ✔ | - | ✔ |
Memory protection | - | ✔ | ✔ |
- |
✔ |
Detection of dispatch | - | ✔ | ✔ | ✔ | ✔ |
Function | ThreaX, TOPPERS/JSP | embOS | NORTi, uC/OSⅡ, uT-Kernel | osCAN, TOPPERS/ASP | RTA-OSEK |
---|---|---|---|---|---|
OS object | ✔ | ✔ | ✔ | ✔ | - |
Task trace | ✔ | ✔ | ✔ | ✔ | ✔ |
Task analyze | ✔ | ✔ | ✔ | ✔ | ✔ |
OS trace | - | - | - | - | - |
OS analyze | - | - | - | - | - |
Task step | - | - | - | - | - |
Currently executed task display | - | ✔ | ✔ | ✔ | - |
Execution history display | - | - | ✔ | ✔ | - |
Realtime profile | - | - | ✔ | ✔ | - |
Task specification | - | - | ✔ | ✔ | - |
Stack coverage | - | - | - | ✔ | - |
Memory protection |
- |
- |
- |
- |
- |
Detection of dispatch | - | - | - | - | - |
Function | Simulator | E1 | E20 | E10A-USB | E8a | E100 | E200F |
---|---|---|---|---|---|---|---|
OS object | ✔ | ✔ | ✔ (RAM monitor supported2) |
✔ | ✔ | ✔ (RAM monitor supported) |
✔ |
Task trace | ✔ | ✔5 | ✔5 (Large capacity2) |
✔1 | - | ✔ (Large capacity) |
✔ |
Task analyze | ✔ | ✔5 | ✔5 (Large capacity2) |
✔1 | - | ✔ (Large capacity) |
✔ |
OS trace | ✔3 | - | - | - | - | ✔4 | - |
OS analyze | ✔3 | - | - | - | - | ✔4 | - |
Task step | - | ✔ | ✔ | - | - | ✔ | - |
Currently executed task display | - | ✔ | ✔ | - | - | ✔ | - |
Execution history display | - | - | - | - | - | ✔ | - |
Real-time profile | - | - | - | - | - | ✔ | - |
Task specification | - | - | - | - | - | ✔ | - |
Stack coverage | - | - | - | - | - | ✔ | - |
Memory protection | - | - | - | - | - | ✔ | - |
Detection of dispatch | - | - | - | - | - | ✔ | - |
Real-time OS | Microcontrollers | |
---|---|---|
Renesas HI7200/MP | V.1.00 Release 03 or later | SH2A-DUAL |
Renesas HI7750/4 | V.2.02 Release 04 or later | SH-4, SH-4A |
Renesas HI7700/4 | V.2.03 Release02 or later | SH4AL-DSP, SH-3, SH3-DSP |
Renesas HI7000/4 | V.2.02 Release 04 or later | SH-2, SH2-DSP, SH-2A, SH-1 |
Renesas RI600/4 | V.1.00 Release 00 or later | RX Family |
Renesas M3T-MR30/4 | V.4.00 Release 00 or later | M16C/60, M16C/50, M16C/30, M16C/20, M16C/10, M16C/Tiny Series |
R8C Family | ||
Renesas M3T-MR30 | V.3.30 Release 2 or later | M16C/60, M16C/50, M16C/30,M16C/20, M16C/10, M16C/Tiny Series |
Renesas MR8C/4 | V.1.00 Release 00 or later | R8C Family |
Renesas HI1000/4 | v1.05 Release01 or later | H8SX Family |
H8S Family | ||
Smalight OS made by Maxell System Tech Co., Ltd. | V3.10 or later | SH-2, SH-2A |
RX Family | ||
M16C/Tiny, M16C/30 and M16C/60 Series | ||
R8C Family | ||
H8SX Family | ||
H8S Family | ||
H8 Family | ||
ThreadX made by Express Logic, Inc. | G5.1.5.0 | SH-2A |
NORTi made by MiSPO Co., Ltd. | Version4 Release 1.20 | SH-4A, SH-2A |
Version4 Release 4.3G | RX Family | |
Version4 Release 1.14 | H8SX Family | |
H8S Family | ||
osCAN made by Vector Informatik GmbH. | Version 3.05 | M16C/60, M16C/Tiny Series |
RTA-OSEK made by ETAS Co., Ltd. | Version 4.0.0 | SH-2A |
uC/OS-II made by Micrium Inc. | V.2.86 (AN-Renesas-SH7201) | SH-2A |
V.2.89 | RX Family | |
V2.83 (AN-1662) | M16C/60 Series | |
V.2.86 (AN-Renesas-H8S2215R, AN-Renesas-H8S2472, AN-Renesas-H8SX1664) | H8SX Family | |
H8S Family | ||
embOS made by Microcontroller GmbH & Co. KG | Version 3.80g | SH-2A |
Version 3.82b | RX Family | |
CMX-RTX made by CMX Systems Inc. | Version 5.30 | RX Family |
TRON Forum uT-Kernel | v1.00.00 | M16C/62P Group |
TOPPERS Project TOPPERS/ASP | Release 1.3.1 | SH-2A |
Release 1.3.2 | M16C/60 Series | |
TOPPERS Project TOPPERS/JSP | Release 1.4.3 | H8/3048 Group |
H8S/2350 Group |
Debugger | Supported microcontrollers | Supported debugger version |
---|---|---|
Simulator debugger | SuperH Family | V.9.08.00 or later |
RX Family | V.1.00.00 ot later | |
H8SX, H8S and H8 Family | V.5.07.00 or later | |
E1 emulator debugger | RX Family, R8C Family | V.1.00 Release 00 or later |
E20 emulator debugger | RX Family, R8C Family | V.1.00 Release 00 or later |
E10A-USB emulatordebugger | SH-2A, SH-4A, SH4AL-DSP, H8SX Family, | V.3.00 Release 00 or later |
H8S Family | ||
SH2A-DUAL, SH4A-MULTI | V.2.00 Release 00 | |
E8a emulator debugger | M16C Family, R8C Family, H8 Family | V.1.02 Release 00 or later |
E100 emulator debugger | RX Family, M16C Family, R8C Family, | V.1.00 Release00 or later |
H8SX Family | ||
E200F emulator debugger | SH-2A | V.3.00 Release 00 |
*. Please refer to the Emulator pages linked above to get to know the detailed supported MCUs.
*TRON Forum holds the copyright on the uITRON Specification and the uT-Kernel specifications.
*The OSEK/VDX steering committee holds the copyright on the OSEK/VDX specifications.
*TOPPERS is a registered trademark of TOPPERS Project.
*OSEK is a registered trademark of Siemens AG.
*ThreadX is a registered trademark of Express Logic, Inc.
*NORTi is a registered trademark of MiSPO Co., Ltd.
*osCAN is a registered trademark of Vector Informatik GmbH.
*RTA-OSEK is a registered trademark of LiveDevices Co., Ltd.
*Smalight is a registered trademark of Maxell System Tech Co., Ltd.
*uC/OS-II is a trademark of Micrium, Inc.
*embOS is a registered trademark of SEGGER Microcontroller GmbH & Co. KG.
*CMX-RTX is a trademark of CMX Systems Inc.
*The other system names and product names referred to in this document are trademarks or registered trademarks of the respective proprietary companies.
*TRON, ITRON, uITRON, uT-Kernel and OSEK/VDX do not refer to any specific product or products.
High-performance Embedded Workshop Real-Time OS Aware Debugging Information for Users