Collecting environmental data has become more and more important for building, industrial and home applications, as it helps maintain a clean atmosphere and minimizes exposure to toxic and dangerous gases. Good air quality is also very important in factories to ensure a safe production site. This gas sensor solution monitors the existence of these gases and connects the data to the cloud.

Renesas’ 32-bit RX130 MCU is connected to the sensor network by a smart Wi-Fi module to feed the data to a suitable gateway and then connects to the cloud.

Key Features:

  • Easy and fast to integrate 
  • Fast productization due to existing cloud solutions with AWS and an RX MCU
  • Gas sensor with highest sensitivity to gases in the market

Applications: 

  • Factory automation
  • Building automation

Related Products

Product Description Featured Document Ordering
       
Microcontroller      
RX130 Cost optimized high performance microcontroller with enhanced touch key function and 5V operation support Datasheet Select specific device
       
Gas Sensor      
SGAS701 Trace hydrogen sensor Datasheet Buy / Sample
ZMOD4410 Indoor Air Quality Sensor Platform Datasheet Buy / Sample
SGAS711 Flammable gas sensor Datasheet Buy / Sample
       
Buck Regulator      
ISL85415 Wide VIN 500mA synchronous buck regulator Datasheet Buy / Sample
       
LDO      
ISL9001A LDO with low ISUPPLY, high PSRR Datasheet Buy / Sample
       

descriptionDocumentation

file_downloadDownloads