IDT Power Metering Solution Offers Unrivaled Accuracy with Largest Dynamic Range in the Industry
November 30, 2010
SAN JOSE, Calif., November 30, 2010 — Integrated Device Technology, Inc. (IDT®) ( NASDAQ: IDTI), the Analog and Digital Company™ delivering essential mixed-signal semiconductor solutions, today announced that the IDT single-phase energy metering IC has been selected by Gude Analog- und Digitalsysteme GmbH, a leading manufacturer of Power Distribution Units through TCP/IP networks, for use in its Expert Power Meter. Gude selected the IDT energy metering IC because of its high accuracy and wide dynamic range; the widest in the metering industry.
The IDT90E21 is a high-performance energy metering device for single-phase two-wire, single-phase three-wire or electricity meters with anti-tampering mode. It boasts the industry's widest dynamic range of 5000:1, which facilitates measurement over a large current range of 20mA to 100A. The device measures RMS voltage and current, phase angle, voltage frequency, power factor, and mean active, reactive and apparent power.
"Gude is a leading maker of high quality power distribution units," said Dr. Michael Gude, CEO and Founder of Gude Analog- und Digitalsysteme GmbH. "We have very stringent standards on features and performance for our Expert Power Meter products. IDT's power metering solution offers great accuracy over a large range, which is important for our product differentiation and competitive advantage."
"Incorporating IDT's proprietary analog-to-digital converter (ADC) and DSP technologies, we have entered a new market with this innovative power metering product, which has gained customer traction in China, Europe, and beyond. We will continue to deliver complete smart metering solutions that are vital to improving energy efficiency for electricity distribution and consumption worldwide," said Sean Fan, vice president and general manager of IDT.
The IDT90E21 is fully compliant with IEC62052-11, IEC62053-21 and IEC62053-23 specifications for class 1 or class 2 single-phase watt-hour meters or class 2 single-phase var-hour meters. The device is offered in a lead-free 28-lead SSOP package, and is designed for long-term stability over variations in grid and ambient environmental conditions.
About IDT
Integrated Device Technology, Inc., the Analog and Digital Company™, combines analog and digital technology to develop system-level innovations that optimize customers’ applications and enrich the end-user experience. IDT uses its market leadership in timing, serial switching and interfaces, and adds analog and system expertise to provide complete application-optimized, mixed-signal solutions for the communications, computing and consumer segments. Headquartered in San Jose, Calif., IDT has design, manufacturing and sales facilities throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT is accessible at www.IDT.com. Follow IDT on Twitter and Facebook.
###
IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc.
All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.
All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.