With RMS Additive Phase Jitter of Sub-50 fsec, the new Buffers Deliver Best-in-Class Performance in an Extremely Small 2 Millimeter-by-2 Millimeter Package

March 24, 2015

SAN JOSE, Calif., March 24, 2015-- Integrated Device Technology, Inc. (IDT®) (NASDAQ: IDTI) introduced today a new family of clock buffers that deliver best-in-class jitter performance in a compact package. The 5PB11xx family of LVCMOS fanout buffers provides low-jitter metrics of sub-50 fsec RMS additive phase jitter (12KHz to 20MHz), offering system designers greater jitter margin than competitive products to help them meet system clock requirements. The small die size enables the chip to fit within a DFN 8-pin package as small as 2 by 2 millimeters.

The buffers are ideal for high-end consumer, industrial, data communications, telecommunications and computing applications where both timing budget and board space are at a premium.

The new buffers are available with 2, 4, 6, 8 and 10 LVCMOS outputs and can support 1.8V, 2.5V and 3.3V power supplies and outputs. They have a low output skew of 50 psec with only 14mA core current consumption. All the devices in the new buffer family are characterized at an extended temperature of -40C to 105C enabling the new buffers to meet the requirements of automotive infotainment applications as well.

“As designs become more complex with tighter timing requirements, jitter will only grow as an obstacle for system designers,” said Dave Shepard, vice president and general manager of IDT’s Timing and RF Division. “Our 5PB11xx fanout buffers give these engineers more elbow room so they can continue to innovate while meeting stringent jitter demands.”

Along with the 5PB11xx family, IDT has introduced a 551S and 553S 1:4 LVCMOS fanout buffer series with sub-50 fsec additive jitter in industry-standard 551 and 553 footprints. These devices are also available in 2-by-2-millimeter DFN 8-pin packages and support 1.8V, 2.5V and 3.3V power supplies and outputs.

Pricing and Availability

The new cost-competitive buffers start at $0.8 for 1K pricing and are available within a short lead time.

About IDT Clock and Timing Solutions

With a product portfolio 10 times greater and broader than any other, IDT is the world’s leader in silicon timing and is in a unique position to address the needs of virtually any application. With the industry’s largest market share, IDT is the only one-stop-shop for timing, offering products from full-featured system solutions to simple clock building-block devices. Factory-programmable options and clock solution customization capabilities address unique customer requirements, while the lowest jitter and lowest power features set IDT apart from the competition. Products are accompanied by a world-class support team driven by service and responsiveness goals. For more information about IDT’s leading portfolio of timing products, please visit www.idt.com/go/timing.

About IDT

Integrated Device Technology, Inc. develops system-level solutions that optimize its customers' applications. IDT uses its market leadership in timing, serial switching and interfaces, and adds analog and system expertise to provide complete application-optimized, mixed-signal solutions for the communications, computing and consumer segments. Headquartered in San Jose, Calif., IDT has design, manufacturing, sales facilities and distribution partners throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol "IDTI." Additional information about IDT is accessible at www.IDT.com. Follow IDT on FacebookLinkedInTwitterYouTube and Google+.

IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.

Share this news on