IDT’s Comprehensive Offering of Communication Signal Chain Products and Innovative Technology Enable Engineers to Solve Phase Noise-related Challenges and Build Cutting-edge Systems

June 20, 2013

SAN JOSE, Calif., June 20, 2013 – Integrated Device Technology, Inc. (IDT®) (NASDAQ: IDTI), the Analog and Digital Company™ delivering essential mixed-signal semiconductor solutions, today announced a low-noise timing chipset optimized for use in wireless base transceiver station (BTS) radio cards. The new chipset complements IDT’s extensive communication signal chain portfolio, offering engineers the tools needed to solve phase noise-related challenges and build cutting-edge wireless systems.

          The IDT 8V19N4xx chipset is a flexible JESD204B-compliant radio frequency phase-locked loop (RF PLL) and clock synthesizer, designed to meet both the high frequency and low phase noise requirements for 2G, 3G and 4G LTE wireless infrastructure. Leveraging IDT’s proven FemtoClock® NG technology, the low phase noise characteristics enable the system’s analog-to-digital and digital-to-analog converters (ADCs / DACs) to function with high precision and very low distortion levels. This results in improved signal integrity on transmission and enhanced signal sensitivity on reception, increasing data throughput via lower bit error rates (BER). Furthermore, reduced noise in the RF signal path enables base-station developers to decrease cost and complexity by relaxing the system’s filter requirements.

          “At IDT, we recognize the undesired effects noise can cause in the RF signal chain, and have developed this timing chipset to provide system engineers a new tool to address it,” said Christian Kermarrec, vice president and general manager of the Timing and Synchronization Division at IDT. “Our new chipset also offers several key features, such as JESD-compliant clocking and integrated clock jitter attenuation for easy integration into our customers' specific architectures. The new timing devices complement our industry-leading timing portfolio as well as our performance-leading data converters, data compression, RapidIO®, and RF signal chain products for wireless infrastructure applications.”

          The IDT 8V19N4xx chipset generates synchronized and highly configurable clock and SYSREF signals as required by JESD204B applications. This allows customers to use a standard, cost-effective timing chipset with a high degree of flexibility instead of multiple PLLs, synthesizers, and buffers. In addition, the devices feature integrated clock jitter attenuation to simplify system design, and support a low-cost, low-frequency external VCXO to reduce system cost.

Product Availability
          The IDT 8V19N4xx devices are currently sampling to qualified customers and are available in standard VFQFPN packages. The RF PLL and high-frequency synthesizer can be paired with other devices for added flexibility in the application. For more information about IDT’s leading clock ICs and timing solutions, please visit www.idt.com/go/timing.

About IDT Clock and Timing Solutions

          With a product portfolio 10 times greater and broader than any other, IDT is the world’s leader in silicon timing and is in a unique position to address the needs of virtually any application. With the industry’s largest market share, IDT is the only one-stop-shop for timing, offering products from full-featured system solutions to simple clock building-block devices. Factory-programmable options and clock solution customization capabilities address unique customer requirements, while the lowest jitter and lowest power features set IDT apart from the competition. Products are accompanied by a world-class support team driven by service and responsiveness goals. IDT has also expanded its portfolio to include frequency control products, such as the XpressO® oscillators from Fox Electronics and an innovative line of MEMS oscillators that are rapidly replacing legacy quartz-based oscillators. For more information about IDT’s leading portfolio of timing products, please visit www.idt.com/go/timing.

About IDT

          Integrated Device Technology, Inc., the Analog and Digital Company™, develops system-level solutions that optimize its customers’ applications. IDT uses its market leadership in timing, serial switching and interfaces, and adds analog and system expertise to provide complete application-optimized, mixed-signal solutions for the communications, computing and consumer segments. Headquartered in San Jose, Calif., IDT has design, manufacturing, sales facilities and distribution partners throughout the world, with direct purchase services through IDT Direct™. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT is accessible at www.IDT.com. Follow IDT on Facebook, LinkedIn, Twitter, and YouTube.

###

IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.

Share this news on