The Semiconductor Company’s Innovative Products Enable The Mobile Internet  

February 18, 2015

SAN JOSE, Calif., Feb. 18, 2015-- Integrated Device Technology, Inc. (IDT®) (NASDAQ: IDTI) announced today that it will showcase its leading wireless technology in early March at Mobile World Congress 2015 in Barcelona. IDT will have demos of its latest wireless power semiconductors as well as products for its wireless infrastructure applications. IDT will display the technology at Booth 1H10. The conference runs March 2 -5 at the Fira Gran Via.

IDT’s wireless power transmitters and receivers have been designed into a wide variety of applications, including smart phones, wearables, charging stations and furniture. The company offers semiconductors that support the three major standards groups: the Wireless Power Consortium (WPC), the Power Matters Alliance (PMA), and Alliance for Wireless Power (A4WP), for both magnetic induction and magnetic resonance charging.

In the area of wireless infrastructure, IDT will showcase its RapidIO interconnect technology, used to connect base station traffic throughout LTE deployments globally, with multiple switch semiconductors per base station. IDT’s RapidIO products can also serve as a gateway between processing elements to enable the hyper-fast movement and management of data in high-performance computing systems.

About IDT

Integrated Device Technology, Inc. develops system-level solutions that optimize its customers’ applications. IDT uses its market leadership in timing, serial switching and interfaces, and adds analog and system expertise to provide complete application-optimized, mixed-signal solutions for the communications, computing and consumer segments. Headquartered in San Jose, Calif., IDT has design, manufacturing, sales facilities and distribution partners throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT is accessible at www.IDT.com. Follow IDT on Facebook, LinkedIn, Twitter, YouTube and Google+.

IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.

Share this news on