The IDT F0480 Simplifies Design of Radio Frequency Variable Gain Amplifier Function While Making Implementation More Reliable
November 12, 2014

SAN JOSE, Calif., Nov. 12, 2014 – Integrated Device Technology, Inc. (IDT®) (NASDAQ: IDTI) today introduced the F0480, an internally matched 400 to 2700 MHz broadband radio frequency (RF) variable gain amplifier (VGA) designed to simplify the design process while ensuring a more reliable implementation. The device delivers exceptional RF performance by combining IDT’s unique Glitch-FreeTM digital step attenuator, and Zero-DistortionTM technologies in a compact 5x5 package.

The chip offers better moisture sensitivity and protection from electrostatic discharge (ESD) for a more robust and reliable technology than Gallium arsenide (GaAs) devices, which require external matching and can suffer from delayed secondary avalanching. It is ideal for such products as cellular 4G base stations, broadband repeaters, distributed antenna systems and microwave backhaul equipment.

Utilizing these innovative technologies results in an industry-leading VGA with +41 dBm OIP3 with 13dB of maximum gain, a wide 23 dB gain control range with 1 dB step resolution, and a Noise Figure of 4 dB, all while consuming only 100mA of current,

“The IDT F0480 delivers unique capabilities to help engineers meet the stringent requirements when designing-in and implementing RF VGAs,” said Chris Stephens, IDT’s senior director, Wireless Product Definition and Marketing. “Its very low power consumption of less than 500mW eases thermal management requirements, while its internal broadband matching greatly simplifies integration into the system.”

The F0480 has 2kV ESD rating and a moisture sensitivity level (MSL) rating of 1, compared to MSL3 for competing GaAs devices. The device’s flat gain slope vs. frequency counteracts board losses.

About IDT

Integrated Device Technology, Inc. develops system-level solutions that optimize its customers’ applications. IDT uses its market leadership in timing, serial switching and interfaces, and adds analog and system expertise to provide complete application-optimized, mixed-signal solutions for the communications, computing and consumer segments. Headquartered in San Jose, Calif., IDT has design, manufacturing, sales facilities and distribution partners throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT is accessible at www.IDT.com. Follow IDT on Facebook, LinkedIn, Twitter, YouTube and Google+.

###

IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.

Share this news on

Share this news on