Ultra-reliable and latency free, the TW8836 offers industry-leading boot time of less than 500 milliseconds

June 2, 2014
 

MILPITAS, Calif., June 2, 2014 (GLOBE NEWSWIRE) -- Intersil Corporation (Nasdaq:ISIL), a leading provider of innovative power management and precision analog solutions, today announced its latest generation LCD video processor—theTW8836—with both analog and digital video inputs, a built-in scaler and de-interlacer, as well as image enhancement and On Screen Display capabilities in a single-chip, hardware-based solution. Intersil's LCD controller family is the most mature and market-proven product of its type. Designed for ultimate flexibility and quality, the TW8836 can be used to display rear camera video with graphic overlay in less than 500 milliseconds from the start of a vehicle, exceeding government safety regulations. This versatile device can be used in a wide array of infotainment system applications and is optimized for use with today's most popular SoCs.

A photo accompanying this release is available at http://www.globenewswire.com/newsroom/prs/?pkgid=25658

 

The National Highway Traffic Safety Administration announced in March 2014 that "rear-visibility technology" must be implemented as standard equipment in all vehicles under 10,000 pounds starting in 2018, as part of the Kids Transportation Safety Act. The move aims to reduce the number of deaths and injuries caused every year by backup accidents, most involving children or seniors. Specifically, the new law mandates that all new light vehicles sold in the U.S. have the ability to display rear camera video within two seconds from the time that the vehicle is put in the reverse gear. Many experts anticipate that other regions around the world will follow suit by implementing similar laws.

 

The TW8836 is designed to sync to a composite video source, scale and de-interlace the video, and display the image on the LCD panel in less than 500 milliseconds, far exceeding the fast boot requirements outlined in the new U.S. law. Because the TW8836 does not require any external memory, the video is latency free and thus ultra responsive to help increase the backup safety of vehicles. Since the TW8366 is a hardware-based solution, many automotive manufacturers view the LCD video processor as more reliable in terms of fast boot capability and as a more stable video path for the rear camera than competing software-based solutions supported by the main processor. Because the main processors require time for the operating system (OS) to boot up, there is risk to routing the rear camera video through SoCs as any glitch in the software could compromise the reliability and integrity of the backup camera video, resulting in a violation of the new U.S. safety regulation.

 

The TW8836 provides a special BT.656 output path that is independent of the primary LCD scaler path, enabling ultimate system architecture flexibility—the chip can drive the panel directly and show rear camera video while the SoC is booting up. Once the SoC boots up, it can then route the source video to the SoC via the BT.656 path to support overlay of graphics (GUI) on top of the video. The combined video can then be sent back to the TW8836 for display on the LCD via the Open LDI (LVDS) or digital RGB input port. Such features allow the TW8836 to be used in conjunction with the most popular infotainment SoCs in the market.

 

The TW8836 LCD video processor can take virtually any type of video input—including analog composite, S-video, analog RGB, digital RGB and Open LDI (LVDS)—and drive almost any digital LCD panel up to WXGA+ (1366x768) resolution—including transistor-transistor logic (TTL), 1 CH Open LDI (LVDS) and timing controller-less (TCON-less) panels—making it an ideal solution for rear camera display or multiple video source infotainment applications. Due to the extreme flexibility and extensive input and output video support, the TW8836 can be used by automotive OEMs to support a wider variety of both analog and digital video sources, as well as offload the video processing workload from the main processor, allowing the processor to support additional system functionality or the manufacturer may simply use a lower cost processor.

 

The TW8836 helps optimize the system design and overall cost as it supports differential composite inputs, eliminating the need for an external op amp. In addition, the device does not need external DRAM, helping to keep the bill of material (BOM) cost of implementing the LCD video processor relatively low.

 

"Intersil is continuing to break new ground in the automotive space by serving the market with an extremely flexible and reliable LCD video processor solution that can be used to increase the safety of vehicles as well as enhance an infotainment system's ability to support a wide variety video sources at the highest grade quality," said Philip Chesley, vice president of Precision Products at Intersil. "Intersil has been the leader in automotive LCD controller technology for over 10 years, which enables us to best serve our long-standing OEM partners' design requirements and deliver a safer, best-in-class experience for consumers."

 

  • Supports most types of video sources:
    • Selectable differential, pseudo differential, and single-ended input NTSC/PAL analog video decoder for traditional analog composite video sources
    • Triple high-speed ADCs for analog RGB/YPbPr input sources up to 1080p/60 resolution
    • 24-bit digital RGB and 1CH Open LDI (LVDS) inputs to support inputs up to 1080p/60 and 720p/60, respectively, from digital sources like smartphones, GPUs and SoCs

 

  • Flexible panel output to drive virtually any type of LCD panel on the market (up to WXGA+ resolution [1366x768]):
    • Supports TTL output up to 24-bit, with dithering for panels that require 18-bit or 16-bit input
    • Supports 1CH Open LDI (LVDS) output to drive the latest generation of HD LCD panels (up to 1366x768)
    • Integrated Timing Controller (TCON) to drive panels that do not have the TCON circuit built in

 

  • AEC-Q100 grade 2 qualified

 

The TW8836 LCD video processor is available now, priced at $7.15 (USD). For more information on the TW8836, please visit: http://www.intersil.com/products/TW8836.

 

Intersil and the Intersil logo are trademarks or registered trademarks of Intersil Corporation. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.

 


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

Share this news on