IDT PCI Express Switches Help Trenton Support I/O Expansion for up to 18 PCI Express Option Cards
2008年5月14日

 

SAN JOSE, Calf. – May 14, 2008 – IDT® (Integrated Device Technology, Inc.; NASDAQ: IDTI), a leading provider of mixed signal semiconductor solutions, today announced that its PCI Express® (PCIe®) family of switching solutions has been chosen by Trenton Technology, Inc. as the foundation for its newly announced BPX6806 PICMG® 1.3 backplane. This server-class PICMG 1.3 (SHB Express™) backplane supports up to 18 PCIemulti-core, multi-processor and option cards, and offers system scalability for demanding telecommunications, data storage and industrial computing applications.
 
With an architecture optimized for backplane applications, the IDT PCIe switches ensure deterministic latency and maximum throughput for all switch ports and system elements regardless of traffic profile or resource loading. Moreover, the IDT PCIe switches enable the Trenton backplane to maximize performance by providing line rate data throughput for multiple simultaneous peer-to-peer transactions. The IDT family of solutions tapped by Trenton provides the industry’s largest port density and most scalable PCIe system solutions for backplane applications.
 
“This industry conversion trend to PCI Express will continue, and many of our customers are migrating their diverse and demanding computing application to PCI Express, leveraging the high-speed, high-bandwidth and scalability the standard offers,” explained Jim Renehan, director of marketing and business development at Trenton Technology. “Our backplane, powered by IDT PCI Express switching technology, provides the PCI Express backplane expansion needed by our customers, while ensuring the highest performance, lowest latency and most reliable PCI Express interfaces possible.”
 
“At IDT, we continue to extend our leadership position in the PCIe switching industry by offering the solutions to enable our customers, such as Trenton, to develop their systems with differentiated features,” said Kam Eshghi, director of marketing for the IDT Serial Switching Division. “Through our conversations with customers, we’re seeing an increased demand for server-class backplanes. Our collaboration with Trenton, as well as other leaders in this space, has allowed IDT to meet this demand by developing switching solutions specifically designed for the needs of this market.”
 
About IDT PCI Express Offerings
IDT provides the broadest range of low power switching solutions targeting system interconnect and system I/O connectivity requirements. In addition, IDT is the leading PCIe timing solutions provider. IDT is an active member of the PCIe special interest group (SIG), and has strategic product plans based upon the standard. For further information about IDT PCIe switching solutions, please go to www.IDT.com/go/PCIe.
 
With the goal of continuously improving the digital media experience, IDT integrates its fundamental semiconductor heritage with essential innovation, developing and delivering mixed signal solutions that solve customer problems. Headquartered in San Jose, Calif., IDT has design, manufacturing and sales facilities throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT is accessible at www.IDT.com.
 
About Trenton Technology
Trenton is a specialized designer and manufacturer of system host boards, single board computers and backplanes for critical embedded computing applications, such as telephony, imaging, instrumentation, control and others that require performance, precision and reliability. As an Associate Member of the Intel® Embedded and Communications Alliance, a community of communications and embedded developers and solution providers, Trenton has the development expertise to provide faster time-to-market designs for the applied computing marketplace. For more information about the Intel® Embedded and Communications Alliance, please visit www.intel.com/go/ica.
 
Trenton offers PCI Express, PCI-X/PCI/ISA and CompactPCI® products manufactured in the USA to ISO 9001:2000, CE and UL standards, satisfying the industry’s increasing demands for features and performance. All Trenton Technology PICMG 1.3 products are backed by a full five-year warranty and Trenton’s engineer oriented technical support.
 
For more information about our BPX6806 backplane, or any other Trenton product, call (800) 875-6031 or (770) 287-3100. You can also visit our website at www.TrentonTechnology.com or e-mail us at Info@TrentonTechnology.com.
 
###
 
IDT and the IDT logo are trademarks of Integrated Device Technology, Inc. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.

分享此文章

分享此文章