IDT Capacitive Touch Controller IC Chosen for its Ultra-Low Power Consumption, Intuitive Interface and Ease of Use
SAN JOSE, Calif., February 24, 2011 – Integrated Device Technology, Inc. (IDT®; NASDAQ: IDTI), the Analog and Digital Company™ delivering essential mixed-signal semiconductor solutions, today announced that its PureTouch® capacitive touch controller has been selected for use in the Hanvon WISEreader, a popular e-book reader based on e-ink technology, which results in a paper-like visual effect for the user. Hanvon is a leading e-book provider in China.
The Hanvon WISEreader utilizes two IDT LDS6107 devices to enable touch-based page forward and page back control sliders, leveraging the built in PureTouch slider function. IDT’s device offers optimized state-machine- and register-based configuration for easy implementation, while the ultra-low power consumption specifications make it ideal for the extended battery life requirements of e-books.
“We are thrilled to partner with Hanvon on this innovative product,” said Alvin Wong, general manager of the IDT Advanced User Interface group. “Our PureTouch controller’s built-in slider function and flexible interface options are a perfect fit for Hanvon’s WISEreader. The device has empowered Hanvon’s system designers to create a streamlined, attractive and reliable product design.”
“The IDT PureTouch controller was an ideal solution for our WISEreader,” said Mr. Wang Bangjiang, vice president at Hanvon. “We wanted to provide our customers with an advanced device that was easy to use and with low power consumption. Using the IDT PureTouch controller for our slider accomplished both these goals.”
About IDT Touch Solutions
IDT is a leading provider of touch controller solutions for consumer, commercial and industrial applications. The IDT PureTouch portfolio of capacitive touch controller devices offers an integrated touch controller that combines the functionality of multiple discrete components into an optimized application-specific solution. The IDT touch technology focuses on reducing board space and improving power consumption, as well as providing enhanced sensory feedback. For additional information on IDT touch solutions, visit www.idt.com/go/touch.
About IDT
Integrated Device Technology, Inc., the Analog and Digital Company™, combines analog and digital technology to develop system-level innovations that optimize customers’ applications and enrich the end-user experience. IDT uses its market leadership in timing, serial switching and interfaces, and adds analog and system expertise to provide complete application-optimized, mixed-signal solutions for the communications, computing and consumer segments. Headquartered in San Jose, Calif., IDT has design, manufacturing and sales facilities throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT is accessible at www.IDT.com. Follow IDT on Facebook, LinkedIn, Twitter, and YouTube.