DRP-Accelerated 2D Barcode Scanning with Renesas RZ/A2M MPUs

Added on 2019-06-20

The DRP coprocessor accelerates 2D barcode detection, extraction, data matrix interpolation, and URL decoding in a live video stream. This is one of six demos Renesas Electronics presented at the Embedded Vision Summit 2019 in Santa Clara, CA, highlighting the capabilities of RZ/A and RZ/G MPUs for low-power, high-performance machine vision systems.