SmartBond™ DA14695 Bluetooth Low Energy 5.2 Development Kit Pro
The DA14695 Development Kit Pro is ideal for software developers who want total control over their software development and want to keep an eye on the power consumption...
The Renesas SmartBond™ Flash Programmer tool lets the user program a flash device for the DA1453x, DA14585/586, and DA1469x SoCs (System on Chip).
This tool allows the user to:
|
|
|
---|---|---|
分類 | タイトル | 日時 |
ソフトウェア/ツール-ソフトウェア | ZIP 9 KB | |
ソフトウェア/ツール-ソフトウェア | MSI 7.12 MB | |
ソフトウェア/ツール-ソフトウェア | ZIP 817 KB | |
3 items
|
The DA14695 Development Kit Pro is ideal for software developers who want total control over their software development and want to keep an eye on the power consumption...
This USB development kit gives users the flexibility to develop applications in a small and portable form factor. The USB board has an on-board debugger, which in...
The DA14531 SmartBond TINY™ Development Kit Pro (DA14531-00FXDEVKT-P) is the most ideal way to quickly and easily get started developing applications and products using...
The DA14531 SmartBond TINY™ USB Development Kit gives you all the flexibility to develop applications in a small and portable form factor.
This kit offers a low-cost...
DA14592-016FDEVKT-P Bluetooth Low Energy Development Kit Proには、マザーボード、ドーターボード、ケーブルが含まれています。 このキットは、ソフトウェアアプリケーションの開発と電力測定に特化して設計されています。
DA14592は...